Hi,
I am trying to use the ‘custom detector’ module in zed-examples/tutorials/tutorial 6 - object detection/ as shown in [zed-examples/tutorials/tutorial 6 - object detection at master · stereolabs/zed-examples · GitHub]
There are two windows, one is the birds view, which shows the 2D image of the left eye. It works well while another one called ‘Zed Object Detection’ window is blank, as follows:
This window is used to show the point cloud and I guess if it’s caused by the problem of OpenGL. The terminal shows:
UserWarning: A NumPy version >=1.16.5 and <1.23.0 is required for this version of SciPy (detected version 1.24.2 warnings.warn(f"A NumPy version >={np_minversion} and <{np_maxversion}"
UserWarning: torch.meshgrid: in an upcoming release, it will be required to pass the indexing argument. (Triggered internally at …/aten/src/ATen/native/TensorShape.cpp:2894.) return _VF.meshgrid(tensors, **kwargs) # type: ignore[attr-defined]
QObject::moveToThread: Current thread (0x56519a0afbe0) is not the object’s thread (0x565191cceab0).
Cannot move to target thread (0x56519a0afbe0)
I wonder what can I do to solve this problem.By the way, I tried the ‘image viewer’ module with python(object_detection_image_viewer.py). It worked well and can detect person. So, I am also doubt that my detection of the other class(trepang) may cause this problem. Also, the YOLOv5 works well and can detect the class of trepang.
I look forward your help and reply, thank you!