The problem of saving point clouds generated by ZED spatial mapping

Hello, I am a student studying ZED spatial mapping. I am using ZED2’s spatial mapping routine to collect point cloud data in real-time. I can see the effect of real-time collection, but it seems that it cannot save the generated point cloud, or I have overlooked it somewhere.

///////////////////////////////////////////////////////////////////////////
//
// Copyright (c) 2024, STEREOLABS.
//
// All rights reserved.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
//
///////////////////////////////////////////////////////////////////////////

/**********************************************************************************
 ** This sample demonstrates how to capture a live 3D reconstruction of a scene  **
 ** as a fused point cloud and display the result in an OpenGL window.           **
 **********************************************************************************/

// ZED includes
#include <sl/Camera.hpp>

// Sample includes
#include "GLViewer.hpp"

#include <opencv2/opencv.hpp>

// Using std and sl namespaces
using namespace std;
using namespace sl;

//#define BUILD_MESH 1

void parse_args(int argc, char **argv,InitParameters& param, sl::Mat &roi);

void print(std::string msg_prefix, sl::ERROR_CODE err_code = sl::ERROR_CODE::SUCCESS, std::string msg_suffix = "");

int main(int argc, char **argv) {

    Camera zed;
    // Set configuration parameters for the ZED
    InitParameters init_parameters;
    init_parameters.depth_mode = DEPTH_MODE::NEURAL;
    init_parameters.coordinate_units = UNIT::METER;
    init_parameters.coordinate_system = COORDINATE_SYSTEM::RIGHT_HANDED_Y_UP; // OpenGL's coordinate system is right_handed
    init_parameters.depth_maximum_distance = 8.;

    sl::Mat roi;
    parse_args(argc, argv, init_parameters, roi);

    // Open the camera
    auto returned_state = zed.open(init_parameters);

    if (returned_state != ERROR_CODE::SUCCESS) {// Quit if an error occurred
        print("Open Camera", returned_state, "\nExit program.");
        zed.close();
        return EXIT_FAILURE;
    }

    if(roi.isInit()){
        auto state = zed.setRegionOfInterest(roi, {sl::MODULE::POSITIONAL_TRACKING, sl::MODULE::SPATIAL_MAPPING});
        std::cout<<"Applied ROI "<<state<<"\n";
    }

    /* Print shortcuts*/
    std::cout<<"Shortcuts\n";
    std::cout<<"\t- 'l' to enable/disable current live point cloud display\n";
    std::cout<<"\t- 'w' to switch mesh display from faces to triangles\n";
    std::cout<<"\t- 'd' to switch background color from dark to light\n";

    auto camera_infos = zed.getCameraInformation();

    // Setup and start positional tracking
    Pose pose;
    POSITIONAL_TRACKING_STATE tracking_state = POSITIONAL_TRACKING_STATE::OFF;

    returned_state = zed.enablePositionalTracking();
    if (returned_state != ERROR_CODE::SUCCESS) {
        print("Enabling positional tracking failed: ", returned_state);
        zed.close();
        return EXIT_FAILURE;
    }

    // Set spatial mapping parameters
    SpatialMappingParameters spatial_mapping_parameters;
    // Request a Point Cloud
#if BUILD_MESH
    spatial_mapping_parameters.map_type = SpatialMappingParameters::SPATIAL_MAP_TYPE::MESH;
    Mesh map;
#else
    spatial_mapping_parameters.map_type = SpatialMappingParameters::SPATIAL_MAP_TYPE::FUSED_POINT_CLOUD;
    FusedPointCloud map;
#endif
    // Set mapping range, it will set the resolution accordingly (a higher range, a lower resolution)
    spatial_mapping_parameters.set(SpatialMappingParameters::MAPPING_RANGE::SHORT);
    spatial_mapping_parameters.set(SpatialMappingParameters::MAPPING_RESOLUTION::HIGH);
    // Request partial updates only (only the last updated chunks need to be re-draw)
    spatial_mapping_parameters.use_chunk_only = true;
    // Stability counter defines how many times a stable 3D points should be seen before it is integrated into the spatial mapping
    spatial_mapping_parameters.stability_counter = 4;

    // Timestamp of the last fused point cloud requested
    chrono::high_resolution_clock::time_point ts_last; 

    // Setup runtime parameters
    RuntimeParameters runtime_parameters;
    // Use low depth confidence to avoid introducing noise in the constructed model
    runtime_parameters.confidence_threshold = 50;

    auto resolution = camera_infos.camera_configuration.resolution;

    // Define display resolution and check that it fit at least the image resolution
    float image_aspect_ratio = resolution.width / (1.f * resolution.height);
    int requested_low_res_w = min(720, (int)resolution.width);
    sl::Resolution display_resolution(requested_low_res_w, requested_low_res_w / image_aspect_ratio);

    Mat image(display_resolution, MAT_TYPE::U8_C4, sl::MEM::GPU);
    Mat point_cloud(display_resolution, MAT_TYPE::F32_C4, sl::MEM::GPU);
    
    // Point cloud viewer
    GLViewer viewer;

    viewer.init(argc, argv, image, point_cloud, zed.getCUDAStream());
 
    bool request_new_mesh = true;

    bool wait_for_mapping = true;

    sl::Timestamp timestamp_start;
    timestamp_start.data_ns = 0;
    

    // Start the main loop
    while (viewer.isAvailable()) {
        
        // Grab a new image
        if (zed.grab(runtime_parameters) == ERROR_CODE::SUCCESS)
        {
            // Retrieve the left image
            zed.retrieveImage(image, VIEW::LEFT, MEM::GPU, display_resolution);
            zed.retrieveMeasure(point_cloud, MEASURE::XYZBGRA, MEM::GPU, display_resolution);
            // Retrieve the camera pose data
            tracking_state = zed.getPosition(pose);
            viewer.updateCameraPose(pose.pose_data, tracking_state);

            if (tracking_state == POSITIONAL_TRACKING_STATE::OK) {
                if(wait_for_mapping){
                    zed.enableSpatialMapping(spatial_mapping_parameters);
                    wait_for_mapping = false;
                }else{
                    if(request_new_mesh){
                        auto duration = chrono::duration_cast<chrono::milliseconds>(chrono::high_resolution_clock::now() - ts_last).count();                    
                        // Ask for a fused point cloud update if 500ms have elapsed since last request
                        if(duration > 100) {
                            // Ask for a point cloud refresh
                            zed.requestSpatialMapAsync();
                            request_new_mesh = false;
                        }
                    }
                    
                    // If the point cloud is ready to be retrieved
                    if(zed.getSpatialMapRequestStatusAsync() == ERROR_CODE::SUCCESS && !request_new_mesh) {
                        zed.retrieveSpatialMapAsync(map);
                        viewer.updateMap(map);
                        request_new_mesh = true;
                        ts_last = chrono::high_resolution_clock::now();
                    }
                }
            }
        }
        map.save("MyMap", sl::MESH_FILE_FORMAT::PLY);
    }

    // Save generated point cloud
    map.save("MyMap", sl::MESH_FILE_FORMAT::PLY);
   
    // Free allocated memory before closing the camera
    image.free();
    point_cloud.free();
    // Close the ZED
    zed.close();

    return 0;
}

void parse_args(int argc, char **argv,InitParameters& param, sl::Mat &roi)
{
    if(argc == 1) return;
    for(int id = 1; id < argc; id ++) {
        std::string arg(argv[id]);
        if(arg.find(".svo")!=string::npos) {
            // SVO input mode
            param.input.setFromSVOFile(arg.c_str());
            param.svo_real_time_mode=true;
            cout<<"[Sample] Using SVO File input: "<<arg<<endl;
        }

        unsigned int a,b,c,d,port;
        if (sscanf(arg.c_str(),"%u.%u.%u.%u:%d", &a, &b, &c, &d,&port) == 5) {
            // Stream input mode - IP + port
            string ip_adress = to_string(a)+"."+to_string(b)+"."+to_string(c)+"."+to_string(d);
            param.input.setFromStream(String(ip_adress.c_str()),port);
            cout<<"[Sample] Using Stream input, IP : "<<ip_adress<<", port : "<<port<<endl;
        }
        else  if (sscanf(arg.c_str(),"%u.%u.%u.%u", &a, &b, &c, &d) == 4) {
            // Stream input mode - IP only
            param.input.setFromStream(String(argv[1]));
            cout<<"[Sample] Using Stream input, IP : "<<argv[1]<<endl;
        }
        else if (arg.find("HD2K") != string::npos) {
            param.camera_resolution = RESOLUTION::HD2K;
            cout << "[Sample] Using Camera in resolution HD2K" << endl;
        }else if (arg.find("HD1200") != string::npos) {
            param.camera_resolution = RESOLUTION::HD1200;
            cout << "[Sample] Using Camera in resolution HD1200" << endl;
        } else if (arg.find("HD1080") != string::npos) {
            param.camera_resolution = RESOLUTION::HD1080;
            cout << "[Sample] Using Camera in resolution HD1080" << endl;
        } else if (arg.find("HD720") != string::npos) {
            param.camera_resolution = RESOLUTION::HD720;
            cout << "[Sample] Using Camera in resolution HD720" << endl;
        }else if (arg.find("SVGA") != string::npos) {
            param.camera_resolution = RESOLUTION::SVGA;
            cout << "[Sample] Using Camera in resolution SVGA" << endl;
        }else if (arg.find("VGA") != string::npos) {
            param.camera_resolution = RESOLUTION::VGA;
            cout << "[Sample] Using Camera in resolution VGA" << endl;
        }else if ((arg.find(".png") != string::npos) || ((arg.find(".jpg") != string::npos))) {
            roi.read(arg.c_str());
            cout << "[Sample] Using Region of intererest from "<< arg << endl;
        }
    }
}

void print(std::string msg_prefix, sl::ERROR_CODE err_code, std::string msg_suffix) {
    cout <<"[Sample]";
    if (err_code != sl::ERROR_CODE::SUCCESS)
        cout << "[Error] ";
    else
        cout<<" ";
    cout << msg_prefix << " ";
    if (err_code != sl::ERROR_CODE::SUCCESS) {
        cout << " | " << toString(err_code) << " : ";
        cout << toVerbose(err_code);
    }
    if (!msg_suffix.empty())
        cout << " " << msg_suffix;
    cout << endl;
}

Hi @zsj520
Welcome to the Stereolabs community.

Is this a modified code, or are you using one of our examples?
Did you get any kind of error when the save function is called?

Please add more information.

Yes, I am using the example of zed-sdk-master\spatial mapping\spatial mapping\cpp,I saw the real-time point cloud and directly closed the interface called ZED Mapping without any errors. The program exited directly, but I did not find the generated point cloud in the space. Is there a problem with my operation

If the application closes correctly you should find the PLY file in the same folder of the executable.
Otherwise, please try to add a printf just before the save command to be sure that it’s called.

How are you closing the application?

I directly clicked on the cross in the upper right corner of the window called ZED Mapping to close the visual window.I tried adding printf on the next saved line, but there was no output.

Select the 3D view window and try to press q or esc to close the program.
It should correctly save the map in this way.

Thank you very much! I have solved my problem.