svo file Playback error

Getting the following error while running svo_playback.py.Same error using C++ file as well.

[ERROR] (../src/sl_input/mmapi/R382/NvV4l2ElementPlane.cpp:370) <p�}> Capture Plane:Getting format: failed: Invalid argument

Traced back the error to the following line input_type.set_from_svo_file(filepath)

svo file recorded using zed 2i NVIDIA Jetson Thor.

Hi @anjan_pivotal
Welcome to the Stereolabs community.

What’s the output of the command ZED_SVO_Editor -inf <svo_filename>?