Support of JetPack 7.2.1 - L4T 39.2.1 for Zed Link Duo - SDK 5.6

Hello everyone,
I have a Jetson AGX Orin 64GB Developer Kit with a Zed Link Duo and 4 ZED X cameras.
I’ve recently updated the AGX Orin to the latest version of JetPack 7.2.1 and L4T 39.2.1.

Since the declared support of the SDK is JetPack 7.2.0 and 39.2, is the installation of the SDK fully compatible? Are there known issues for which it’d make sense to downgrade the JetPack version?

Thanks.

Hi @priva,
welcome to the StereoLabs community

Yes. JetPack 7.2.1 (L4T 39.2.1) is a patch release of JetPack 7.2 with the same CUDA 13.2 branch, so the ZED SDK v5.6 for JetPack 7.2 (L4T 39.2) is the correct installer for your Jetson AGX Orin.

For the ZED Link Duo, install the driver v1.5.0 for L4T 39.2 from the ZED X Drivers page. If dpkg refuses the installation because of the different L4T patch version, you can safely force it:

sudo dpkg -i --ignore-depends=nvidia-l4t-kernel stereolabs-zedlink-duo_1.5.0-LI-MAX96712-L4T39.2.0_arm64.deb

Are there known issues for which it’d make sense to downgrade the JetPack version?

No, we have no known issues that require a downgrade to JetPack 7.2.0.