Hi,
I’m working with two ZED X One GS cameras (SN 307834130 & 300007189) on an NVIDIA Jetson and have lost and wasted a lot of research time fighting a cluster of issues. I’ve tested SDK v5.0.0, v5.0.1, and v5.0.3 plus ZED X Driver v1.3.0 and the brand-new Media Server.
Reproducible problems
- Low, unstable streaming rates far below the specified image & IMU frequencies.
- IMU anomalies
- Y- and Z-axis angular-rate signs inverted
- X-axis shows a periodic noise component (visible in FFT)
- System resets outdoors – Jetson reboots without kernel panic when camera housings overheat.
- Uneven sharpness – left part of every image is noticeably softer than the right on both units.
- Unequal SVO2 compression times
- SN 307834130 ≈ 5.39 ms / frame
- SN 300007189 ≈ 1.91 ms / frame (same compression ratio)
- New with SDK 5.0.3: calibration file generated via
stereo_calibrationno longer works in ZED_Depth_View, although it loads fine in5.0.0/5.0.1.
What I’ve already tried
- Clean installs of SDK 5.0.1 → 5.0.3 and clean rebuilds of sample code.
- Media Server on
127.0.0.1as suggested by support. - Company-supplied calibration procedure & config files.
- Verified issues on both cameras and on two separate Jetson devices.
Why I’m posting
- My original forum threads (links below) haven’t been answered since 29 Apr 2025.
- Email support acknowledged the ticket only after I escalated on 3 Jul 2025 and suggested retrying 5.0.3, which unfortunately introduced an extra regression (calibration file).
- After reporting the issues on 4 Ju 2025 again, they kept slience and didn’t reply to my email.
Previous threads:
• Data streaming frequency - https://community.stereolabs.com/t/data-streaming-frequency/8709
Help needed
- Please do fix the issues and really provide solutions.
Any insights, patches or even confirmation that you see the same behaviour would be hugely appreciated. I’m close to returning the hardware.
Thanks in advance.