Status of Python Multiprocessing Support for ZED X

Hello,

From older threads around 2023–2024, it seems that the ZED X camera had a known bug related to the use of Python’s multiprocessing module.

I’m currently working with the multiple ZED X mini in Python and need to use multiprocessing for
parallel data capture/processing. Before investing more time, I wanted to check:

  1. Has the multiprocessing bug related to ZED X camera been resolved as of 2026?
  2. If so, in which SDK version was this fixed?
  3. Are there any updated best practices or examples for using Multiprocessing with ZED X in Python?

Thank you in advance for any updates or insights!

Best regards,
Ryu

Hi @ryuh1988
Welcome to the Stereolabs community.

Please don’t be vague. A link to the discussions you’re referring to might help us understand the specifics of the issue you’re discussing.

Hi @Myzhar
Thank you for your reply.
The threads I was referring to are listed below. Based on the first one, I understood that a workaround had been identified for the ZED 2i, but no solution had been found for the ZED X at that time.

Python Multiprocessing Bug fix?

ZED X (gmsl) Not working with python multiprocessing

Hello @Myzhar,

Could you please provide a response regarding this issue? I’d really appreciate any guidance.

Thank you!

Hi @ryuh1988
My apologies for the delay.
This is still a work in progress.