Hi
Is there a way to exclude some pixels or rectangle areas frome the stereo frames prior to SLAM processing?
E.g. exclude moving objects related areas in order to make the point cloud of the static world more robust?
Hi
Is there a way to exclude some pixels or rectangle areas frome the stereo frames prior to SLAM processing?
E.g. exclude moving objects related areas in order to make the point cloud of the static world more robust?
Hi Tetsujinfr,
this is not an available feature in the ZED SDK.
However, dynamic objects should already be removed by the process itself, the only thing you can adjust is the depth confidence.
The dynamic objects removal of the SDK is decent from experience, but there are 2 scenarios where I observe (understandably) limitations:
Do not get me wrong, the SDK algo is quite impresssive, but those 2 scenarios limitations are significant robustness issues for my project.
Any chance that a future SDK update can accept those exclusion areas rectangles coord which would be provided by the user? Or something like that?
If you are planning for a deep learning augmented algo I would take that of course, but please note that I use a ZED Mini, which as I understand does not benefit from the work you are doing on the ZED2 for object detection etc.
Thank you for your suggestions. We will consider them for future releases, if compatible with our algorithms.
Those guys from SLAMcore have the dynamic object removal (they say), leveraging neuralnet segmenetation plus rgbd. I guess it is pretty slow and it is not clear which piece is executed realtime and which is not, plus the removal is not perfect (human shoes not removed), but it illustrate well my points above.
At 2’:22"
(The heightmap function is pretty cool too btw)