Hi!
One question, can the SDK 4.2 be used for Jetson Orin Nano with Jetpack 6.1 (L4T 36.4) with CUDA 12.6? The download list only includes JetPack 6.0 (L4T 36.3), Jetson Orin, and CUDA 12.2.
Hi @AnaRubin
the ZED SDK for JP6.1 has not been released yet.
We will release it in the next few weeks
same here. waiting for the support of jetpack 6.1 (36.4) on jetson Orin AGX.
Just a few more days of patience. We hope it will be released next week.
Hi @Myzhar I can see there is 6.1 Jetpack for jetson orin nx, I was wondering if you can share with technical docs how I can update from 6.0 GA to 6.1
Thank you
Hi @nyrjan
if you are using a ZED Box, it does not yet support JP6.1.
We will add an upgrade script as soon as possible.
If you are using an NVIDIA devkit, please refer to the official NVIDIA documentation.
What is the status on jetpack 6.1 with CUDA 12.6?
We are currently testing it for reliability concerning the new SUPER MAX N power mode.