SDK can't detect Camera

Dear StereoLabs Support Team,

I attempted to run a ZED1 camera that was available in my research lab.
(The camera does not have a USB port but is connected with a fixed cable, so I assume it is a ZED1.)

Initially, I was able to run the camera on a desktop running Ubuntu 20.04, and it worked fine.
However, the next day, it completely stopped working in Ubuntu 20.04, and now it is not being detected in any environment:

  • Docker environment
  • My laptop running Ubuntu 20.04
  • My laptop running Windows

I keep getting warnings that I should switch to a USB 3.0 port, but I have already connected the camera to a USB 3.0 port directly (without a hub).

This is driving me crazy.

I am using the latest SDK version 4.2.5 and CUDA 11.8, and everything is properly installed.

I suspect it might be a hardware issue. If so, how can I resolve it?

  • Can the camera be repaired?
  • If I send it in for repair, how long would it take?

I have attached the ZED_Diagnostic_Results.json file for reference.

I look forward to your response.

Thank you.

ZED_Diagnostic_Results.json

{
    "AI Models": {
        "info": [
            "MULTI CLASS DETECTION is not optimized",
            "MULTI CLASS MEDIUM DETECTION is not optimized",
            "MULTI CLASS ACCURATE DETECTION is not optimized",
            "HUMAN BODY FAST DETECTION is not optimized",
            "HUMAN BODY MEDIUM DETECTION is not optimized",
            "HUMAN BODY ACCURATE DETECTION is not optimized",
            "HUMAN BODY 38 FAST DETECTION is not optimized",
            "HUMAN BODY 38 MEDIUM DETECTION is not optimized",
            "HUMAN BODY 38 ACCURATE DETECTION is not optimized",
            "PERSON HEAD DETECTION is not optimized",
            "PERSON HEAD ACCURATE DETECTION is not optimized",
            "REID ASSOCIATION is not optimized",
            "NEURAL DEPTH is not optimized",
            "NEURAL PLUS DEPTH is not optimized"
        ]
    },
    "Camera Test": {
        "InternalDevicesCount": 1,
        "ZEDCount": 0,
        "error": [
            "<b>Camera not detected</b> <br/> Make sure the camera is plugged in or try another USB 3.0 port."
        ]
    },
    "Devices": {
        "ASMediaFound": false,
        "CorruptedFirmware": false,
        "OC_Cam_Detected": false,
        "OtherUSBDevices": [
            {
                "USBMode": 3,
                "USB_path": "/16",
                "bDescriptorType": 1,
                "bDeviceProtocol": 0,
                "bLength": 18,
                "bMaxPacketSize0": 9,
                "bNumConfigurations": 1,
                "bcdDevice": "2.4",
                "bcdUSB": "3.0",
                "bcdUSBClass": 0,
                "bcdUSBSubClass": 0,
                "busNumber": 1,
                "iManufacturer": 1,
                "iProduct": 2,
                "iSerial": 3,
                "idProduct": 790,
                "idVendor": 3034
            }
        ],
        "USBList": [
            {
                "USBMode": 3,
                "USB_path": "/15",
                "bDescriptorType": 1,
                "bDeviceProtocol": 1,
                "bLength": 18,
                "bMaxPacketSize0": 9,
                "bNumConfigurations": 1,
                "bcdDevice": "1.0",
                "bcdUSB": "3.0",
                "bcdUSBClass": 239,
                "bcdUSBSubClass": 2,
                "busNumber": 1,
                "device": "ZED",
                "iManufacturer": 1,
                "iProduct": 2,
                "iSerial": 0,
                "idProduct": "0xf582",
                "idVendor": "0x2b03"
            },
            {
                "USB_path": "/6",
                "idProduct": "0x6005",
                "idVendor": "0x048d"
            },
            {
                "USB_path": "/2",
                "idProduct": "0xc542",
                "idVendor": "0x046d"
            },
            {
                "USB_path": "/8",
                "idProduct": "0xce00",
                "idVendor": "0x048d"
            },
            {
                "USB_path": "/16",
                "idProduct": "0x0316",
                "idVendor": "0x0bda"
            },
            {
                "USB_path": "/10",
                "idProduct": "0x0026",
                "idVendor": "0x8087"
            },
            {
                "USB_path": "/6",
                "idProduct": "0x6005",
                "idVendor": "0x048d"
            },
            {
                "USB_path": "/5",
                "idProduct": "0xb71a",
                "idVendor": "0x04f2"
            },
            {
                "USB_path": "/5",
                "idProduct": "0xb71a",
                "idVendor": "0x04f2"
            }
        ],
        "USBMode": 3,
        "ZED Camera Module Detected": 62850,
        "ZEDDetected": true,
        "captureDevices": [
        ],
        "controllers": [
            {
                "CompatibleIDs": "",
                "Description": "USB �� �\f(USB 3.0)",
                "DeviceName": "",
                "Driver": "{36fc9e60-c465-11cf-8056-444553540000}\\0003",
                "Location": "",
                "Manufacturer": "(\\",
                "Name": "USB",
                "PhysicalName": "\\Device\\USBPDO-1"
            },
            {
                "CompatibleIDs": "PCI\\VEN_8086&CC_0C0330",
                "Description": "USB xHCI ܩ 8�� ��d�",
                "DeviceName": "Intel(R) USB 3.20 U� ",
                "Driver": "{36fc9e60-c465-11cf-8056-444553540000}\\0000",
                "Location": "PCI �� 0, �X 13, 0� 0",
                "Manufacturer": "|\u0018 USB xHCI 8�� ��d�",
                "Name": "PCI",
                "PhysicalName": "\\Device\\NTPNP_PCI0008"
            },
            {
                "CompatibleIDs": "PCI\\VEN_8086&DEV_51ED&REV_01",
                "Description": "USB xHCI ܩ 8�� ��d�",
                "DeviceName": "Intel(R) USB 3.10 U� ",
                "Driver": "{36fc9e60-c465-11cf-8056-444553540000}\\0002",
                "Location": "PCI �� 0, �X 20, 0� 0",
                "Manufacturer": "|\u0018 USB xHCI 8�� ��d�",
                "Name": "PCI",
                "PhysicalName": "\\Device\\NTPNP_PCI0010"
            },
            {
                "CompatibleIDs": "USB\\USB20_HUB",
                "Description": "|\u0018 USB �\f",
                "DeviceName": "",
                "Driver": "{36fc9e60-c465-11cf-8056-444553540000}\\0016",
                "Location": "Port_#0003.Hub_#0002",
                "Manufacturer": "(\\",
                "Name": "USB",
                "PhysicalName": ""
            },
            {
                "CompatibleIDs": "",
                "Description": "USB �� �\f(USB 3.0)",
                "DeviceName": "",
                "Driver": "{36fc9e60-c465-11cf-8056-444553540000}\\0004",
                "Location": "",
                "Manufacturer": "(\\",
                "Name": "USB",
                "PhysicalName": "\\Device\\USBPDO-0"
            }
        ],
        "notTested": [
            "Please connect a camera to test the USB connection."
        ]
    },
    "Graphics Card": {
        "deviceCount": 1,
        "deviceDriverVersion": 12070,
        "devices": [
            {
                "arch": "Ampere",
                "computeCapability": "8.6",
                "cores": 5888,
                "name": "NVIDIA GeForce RTX 3070 Ti Laptop GPU",
                "totalMemoryBytes": "8589410304",
                "totalMemoryMB": 8191.5
            }
        ],
        "initResult": 0,
        "valid": [
            "<b>Graphics card: </b> NVIDIA GeForce RTX 3070 Ti Laptop GPU"
        ]
    },
    "Processor": {
        "OS": "Windows 10 FallCreators",
        "avxSupported": true,
        "coreCount": "14",
        "cpu": "12th Gen Intel(R) Core(TM) i7-12700H",
        "datetime": "2025-02-07 20:07:41",
        "hyperThreading": "1",
        "motherboard": "GM5AG7Y, HANSUNG COMPUTER",
        "ramCapacity": "15.7464",
        "ramUsage": "0",
        "ramUsed": "8.93255",
        "threadCount": "20",
        "valid": [
            "<b>Processor: </b> 12th Gen Intel(R) Core(TM) i7-12700H",
            "<b>Motherboard: </b> GM5AG7Y, HANSUNG COMPUTER"
        ]
    },
    "ZED SDK": {
        "CUDA Toolkit version": "V11.8.89 -->located in C:/Program Files/NVIDIA GPU Computing Toolkit/CUDA/v11.8/bin/nvcc.exe",
        "CUDA loading": false,
        "ZED SDK Version (Diag)": "4.2.5",
        "ZED SDK Version (RT)": "4.2.5",
        "ai": {
            "checkAI": true,
            "cudaVersion": 11080,
            "cudnnCudartVersion": 11080,
            "cudnnVersion": 8907,
            "cudnnVersionExpected": 8907,
            "tensorVersion": 8601
        },
        "binFiles": [
            "cudnn64_8.dll",
            "cudnn_adv_infer64_8.dll",
            "cudnn_adv_train64_8.dll",
            "cudnn_cnn_infer64_8.dll",
            "cudnn_cnn_train64_8.dll",
            "cudnn_ops_infer64_8.dll",
            "cudnn_ops_train64_8.dll",
            "nvinfer.dll",
            "nvinfer_builder_resource.dll",
            "nvinfer_dispatch.dll",
            "nvinfer_lean.dll",
            "nvinfer_plugin.dll",
            "nvinfer_vc_plugin.dll",
            "nvonnxparser.dll",
            "nvparsers.dll",
            "sl_ai64.dll",
            "sl_zed64.dll",
            "zlibwapi.dll"
        ],
        "driverVersion": "566.03",
        "drivervDllVersion": "32.0.15.6603",
        "resourcesFiles": [
        ],
        "resourcesFilesExpected": [
            "objects_performance_3.2"
        ],
        "runtimeDllVersion": 11080,
        "valid": [
            "<b>ZED SDK version:</b> 4.2.5",
            "<b>CUDA version:</b> V11.8.89"
        ]
    }
}

Hi @dahun09021
Welcome to the Stereolabs community

Your camera is correctly detected by your OS.
You can try to open the video stream with a webcam application.

If the stream is not available, then the cable of the camera (an old cable considering the old camera model) is damaged.

In this case you can try to recover the camera by replacing the cable.
You can follow this unofficial guide to open it.

I also encountered this problem and couldn’t find a solution.