I’m encountering an issue where pyzed.sl.CameraOne.get_camera_information() fails when streaming a single (mono) ZED X One camera from a ZED Box Orin to an x86 receiver using SDK 5.0. Image grabbing and retrieval work fine, but the metadata call crashes with a Cython initialization error. I’ve confirmed the .conf calibration file is present and can manually parse it as a workaround, but I’d prefer a proper fix.
Setup Details
-
Camera: Single ZED X One (not stereo pair)
-
Sender: ZED Box Orin (Jetson L4T 36.3).
-
Driver: stereolabs-zedbox-duo_1.3.1-LI-MAX96712-all-ZEDBOX-L4T36.3.0_arm64.deb.
-
SDK: ZED_SDK_Tegra_L4T36.3_v5.0.5.zstd.run.
-
Streaming via ZED Media Server (mono mode) to IP/port.
-
-
Receiver: Ubuntu x86_64.
- Python wheel: pyzed-5.0-cp312-cp312-linux_x86_64.whl.
-
Resolution: HD1080 (1920x1080), FPS: 15.
Minimal Code Example
I have a find_and_open_camera_stream() method:
self.init_params = sl.InitParametersOne() self.init_params.set_from_stream(self.stream_ip, self.stream_port) # e.g., "192.168.x.x", 34000self.init_params.camera_resolution = sl.RESOLUTION.HD1080 self.init_params.camera_fps = 15 self.zed = sl.CameraOne() err = self.zed.open(self.init_params)iferr != sl.ERROR_CODE.SUCCESS: returnFalse # Delay and grab succeedtime.sleep(2)ifself.zed.grab() == sl.ERROR_CODE.SUCCESS: print("Grab successful") # This prints # But this fails camera_info = self.zed.get_camera_information()
Traceback
Traceback (most recent call last): File ".../zed_camera.py", line 167, in find_and_open_camera_stream camera_info = self.zed.get_camera_information(sl.Resolution(0, 0)) ^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^ File "pyzed/sl.pyx", line 14730, in pyzed.sl.CameraOne.get_camera_information File "pyzed/sl.pyx", line 13861, in pyzed.sl.CameraOneInformation.__cinit__ File "pyzed/sl.pyx", line 5495, in pyzed.sl.SensorsConfiguration.__cinit__
What Works
-
Streaming connects fine (
open()succeeds). -
grab()andretrieve_image()return valid RGB images. -
Manual parsing of /usr/local/zed/settings/SN.conf for intrinsics works as a temp fix.
Is this a known bug in SDK 5.0 for mono ZED X One (streaming and/or direct PC connection)?
Thanks!