SCENE_ILLUMINANCE not working with 5.2.3 SDK

after upgrading from 5.1.1 to 5.2.3 I found out that reading the SCENE_ILLUMINANCE is returning -1 instead of the actual LUX of the scene.

is this a bug, or do I need to request it in another way?

We are using this value to automaticlly turning on (extra) work lights to get a beter lightning, so we are really depending on it to get 24/7 autonomous work done.

Hi @Martijn

What tool/framework are you using?

I am using the sdk and build our own application with it.

so jetson jetpack 6.2

I readout the illuminance with follow code:
int illuminance;
zed->getCameraSettings(sl::VIDEO_SETTINGS::SCENE_ILLUMINANCE ,illuminance);

Hi @Martijn
I checked, and this seems to be a bug in ZED SDK v5.2.3.
I reported the problem to the team. It will be fixed with one of the next patches..

Hi @Martijn
I confirm that the fix to this problem will be available with the next ZED SDK release.

I have installed the latest ZED SDK 5.3.0
But I still get -1 as lux value.

I use ZED X camera’s on a jetson.

When Could we expect a fix for it?

I reported the problem to the ZED SDK team. A fix is expected with the next v5.3.1 patch release