Hello everyone,
I’ve successfully trained a custom model using YOLOv5 and loaded it using torch.hub.load. Following the Stereolabs tutorial here, I have a couple of questions:
- I’ve detected objects and passed their information to the
ingest_custom_box_objectsfunction, but I’m uncertain about its actual effect. How can I visualize the impact of this function? - After using the
ingestfunction, I attempted to access the positions of detected objects usingobjects = sl.Objects()andzed.retrieve_objects(objects, obj_runtime_param)sa tutorial says. However, when checkingobjects.object_list, it appears to be null. How can I retrieve the positions of my detected objects with my custom model?
You can see the code below.
Thank you for your assistance.
import pyzed.sl as sl
from typing import Any
import numpy as np
import torch
import cv2
import time
def init_zed():
zed = sl.Camera()
init_params = sl.InitParameters()
init_params.coordinate_units = sl.UNIT.METER
init_params.camera_resolution = sl.RESOLUTION.HD1080
init_params.camera_fps = 30
err = zed.open(init_params)
if err != sl.ERROR_CODE.SUCCESS:
print(repr(err))
zed.close()
exit(1)
else:
print("Zed Camera Started!")
return zed
def load_model(model_name):
model = torch.hub.load("ultralytics/yolov5","custom", path=model_name, force_reload=True)
return model
def detector(model,frame,device):
model.to(device)
frame = [frame]
results = model(frame)
labels, cord = results.xyxyn[0][:, -1], results.xyxyn[0][:, :-1]
return labels, cord
def main():
model_name = "model/yolov5/bestModel.pt"
device = 'cuda' if torch.cuda.is_available() else "! cpu"
# İnitalizing zed and setting parameters
zed = init_zed()
runtime_params = sl.RuntimeParameters()
image_left = sl.Mat()
depth_left = sl.Mat()
point_cloud = sl.Mat()
# Setting object detection parameters
obj_params = sl.ObjectDetectionParameters()
obj_params.detection_model = sl.OBJECT_DETECTION_MODEL.CUSTOM_BOX_OBJECTS
zed.enable_object_detection(obj_params)
obj_runtime_params = sl.ObjectDetectionRuntimeParameters()
model = load_model(model_name)
while True:
if zed.grab(runtime_params) == sl.ERROR_CODE.SUCCESS:
zed.retrieve_image(image_left, sl.VIEW.LEFT)
zed.retrieve_measure(depth_left, sl.MEASURE.DEPTH)
zed.retrieve_measure(point_cloud, sl.MEASURE.XYZRGBA)
image = image_left.get_data()
labels, cords = detector(model, image, device)
labelL = lables.tolist()
cordL = cords.tolist()
objects_in = []
# The "detections" variable contains your custom 2D detections
for label, cord in zip(labelL, cordL):
tmp = sl.CustomBoxObjectData()
# Fill the detections into the correct SDK format
tmp.unique_object_id = sl.generate_unique_id()
tmp.probability = cord[4]
tmp.label = int(label)
xmin, ymin, xmax, ymax, conf = cord
# Convert to [top-left, top-right, bottom-right, bottom-left]
top_left = [xmin, ymin]
top_right = [xmax, ymin]
bottom_right = [xmax, ymax]
bottom_left = [xmin, ymax]
tmp.bounding_box_2d = np.array([top_left, top_right, bottom_right, bottom_left])
tmp.is_grounded = True
objects_in.append(tmp)
zed.ingest_custom_box_objects(objects_in)
objects = sl.Objects() # Structure containing all the detected objects
zed.retrieve_objects(objects, obj_runtime_params) # Retrieve the 3D tracked objects
for object in objects.object_list:
print("{} {}".format(object.id, object.position))