hi, i want to record depth data using sl::Mat object and save it locally. first of all how would i do that? second, if i do that and then want to load this data and change the DEPTH mode post, i.e recording in ULTRA and then running NEURAL, would it be possible? if so how?
svo i what we were using until now but it is not efficient for us to export it every time, it take a lot of time for our large datasets to process the svo and so we want to record all necessary data directly to hdf5 format, what i needed from you is to know if i load it again to sl::Mat format from my hdf5 will i be able to rum lets say NEURAL depth mode if i recorded data in ULTRA Depth mode for example and if so how?
We do not support the hdf5 format.
You must write your converter for that.
Furthermore, you cannot convert a depth map saved with ULTRA mode into a depth map in NEURAL mode. Only SVO files allow you to generate the two different depth maps from the same input data.
this is what igot for example:(base) nir@nir:~/Desktop$ /usr/local/zed/tools/ZED_SVO_Editor -inf top_camera_blue_4.svo
-inf option detected
SVO Infos :
Image Size : [ 1920 x 1080 ]
Framerate : 30
Number of Frames : 271
ZED Serial Number : 55187685
Compression mode : " H264 Lossy (GPU) compression"
Product : ZED-XM
Sensors Fw version : 1000
Camera Fw version : 2001
is there a way to get the info of the timestamps and frames mapping?