I am using a ZED X Mini with a Jetson development board, and I am using the Python ZED SDK.
I use zed.grab() to acquire RGB images, depth visualization (depth_vis), and raw floating-point depth data.
I found that at SVGA resolution, a single retrieve_measure() call takes about 20–25 ms. Is this normal?
At HD1080 resolution, it takes even longer, making it difficult to achieve a 30 FPS capture rate.
Is this expected behavior?
Strictly speaking, it is retrieve_measure to slow
Hello @timsaya,
As the majority of ZED SDK algorithms are computed in the grab() method, the latency of the grab() call depends on the following:
- resolution / frame rate selected
- which depth mode is enabled (NEURAL, NEURAL_PLUS, etc)
- if there are other algorithms (positional tracking, object detection, etc) enabled
- the compute unit used (embedded Jetson computer or x86 PC with a big GPU)
- the power mode used for Jetson devices (recommended is MAXN for the fastest compute)
Which jetson platform are you using?
Jetson Orin NX 8GB
Is 20–30 ms expected? Is it possible to get it down to 10 ms on C++ SDK ?