Python : keep data in GPU

Hello,

I developed some CUDA processing for the depth data sl.MEASURE.XYZRGBA.

I would like to avoid moving data from GPU (I expect data to be computed on GPU by ZED SDK) then to CPU and then go back to GPU.

I tried to set cam.retrieve_measure(ptCloud, sl.MEASURE.XYZRGBA , sl.MEM.GPU) then I have an error as attribute GPU does not exist (which is used on this page : Using the Depth Sensing API | Stereolabs )

How could i keep data on GPU to avoid extra transfer that cost lots of time ?

Regards

Boris

Hello,

Indeed, you cannot keep the memory on the GPU with our Python wrapper. We did not find a way to do this (yet).
However our wrapper is open source (GitHub - stereolabs/zed-python-api: Python API for the ZED SDK)
You are more than free to give us any idea you can have about this kind of CUDA usage in python.

Antoine

Hello,

So we recently wanted to achieve the same, and I went down the rabbit hole of trying to figure this out.
I think I got an answer to this issue, and I already raised a PR: https://github.com/stereolabs/zed-python-api/pull/230) containing the changes.

It’s still not thoroughly tested, but I kinda want the community to take it from here.

Great,

I hope I will be able to test it soon.
Did you check if it is possible to use sl.MEM.GPU with the latest version of the SDK ( 4.0 ) ?
The documentation does not mention any restriction with it.

Actually, I worked on the 4.0, and the Python API still had no sl.MEM.GPU option. Additionally, the Python API only returned Numpy arrays (only CPU).

Hello! Has there been any progress on this? I saw the PR, has this been integrated after the latest 4.1 sdk release? Any other way around this?
Thanks a lot and really appreciate the effort!!!

I recently opened a new PR with full working GPU grab across all resolutions (tried it even with the ZED X Mini with HD1200 resolution). It works with ZED SDK 4.1.4.
You can give it a try and see if it suits your needs: get_data on GPU using cupy by Rad-hi · Pull Request #241 · stereolabs/zed-python-api · GitHub