Machine used: ZED BOX ORIN NX
Camera model: ZED2i connected.
Ubuntu version / ROS Version: Ubuntu 20.04 / ROS Noetic
Greetings, I was checking ZED documentation and saw that the parameter pub_frame_rate should be published as dynamic, but I don’t see it in rqt and neither in the cfg file where all the dynamic params are being defined.
I tried to search if for some reason, this param is not dynamic anymore, but with no results. I imagine this feature was once available because I saw a related GitHub issue ([BUG] dynamic parameter pub_frame_rate missing? · Issue #593 · stereolabs/zed-ros-wrapper · GitHub). It would be interesting since we would like to test the performance of the system and test different pub frequencies to see which would be the best. Thanks from advance