Problems with ZEDX Driver install on encrypted drive on Jetson

Hi, I’m reporting a problem with the stereolabs driver install on a Jetson Orin NX.
I’m trying to install stereolabs-zedlink-mono_1.3.0-SL-MAX9296-all-L4T36.3.0_arm64.deb on a Jetson Orin NX running Jetpack 6.0, where the filesystem is flashed on an encrypted partition of the NVME SSD.
I have successfully installed this on an unencrypted SSD flashed using SDKmanager. However, when flashing and applying encryption I have to use the Nvidia scripts, and the resulting partitions are different.

On an encrypted drive we have 2 partitions:

nvme0n1        259:0    0 931.5G  0 disk  
├─nvme0n1p1    259:1    0   400M  0 part  /boot
├─nvme0n1p2    259:2    0  24.6G  0 part  
│ └─crypt_root 253:0    0  24.6G  0 crypt /

ie / and /boot are in different partitions.
fstab looks like this:

PARTUUID=<UUID> /boot ext4 defaults 0 1
/dev/mapper/crypt_root / ext4 defaults 0 1
/dev/mapper/crypt_UDA /mnt/crypt_UDA ext4 defaults 0 2

When I unpack the stereolabs dpkg, it writes an entry to the extlinux.conf that looks like this:

LABEL Stereolabs
        MENU LABEL Stereolabs kernel
        LINUX /boot/Image
        FDT /mnt/APP/boot/dtb/kernel_tegra234-p3768-0000+p3767-0000-nv.dtb
        INITRD /boot/initrd
        APPEND ${cbootargs} root=UUID=<UUID> rw rootwait rootfstype=ext4 mminit_loglevel=4 console=ttyTCU0,115200 firmware_class.path=/etc/firmware fbcon=map:0 net.ifnames=0 nospectre_bhb video=efifb:off console=tty0
        OVERLAYS /boot/tegra234-p3768-camera-zedlink-mono-sl-overlay.dtbo

Here the FDT line is incorrect - there is no /mnt/APP mountpoint. When the system boots it doesn’t find the FDT file and hence the Stereolabs overlay isn’t loaded.
To fix this I have to edit the //boot/extlinux.conf to remove the /mnt/APP prefix.
This prefix is introduced by the board.py script in /boot/stereolabs/utils/Jetson, which thinks the system is an NFS mount and is incorrectly mounting / to /mnt/APP as in function _board_partition_mount().
Could you investigate and resolve please?

Note that changing /mnt/APP/boot/ to /boot/ on that FDT line (and moving the Stereolabs DTBOs into the same folder as the other DTBOs and symlinking appropriately) allows the Orin to boot and allows the ZEDX driver to start.

Hi,
Thank you for your detailed feedback we will update the script taking into account this particular setup. Your current fix should be good, this is the same configuration that we will apply