Problems in using Body tracking in SDK 4.0

Hello,
I am trying to use the new SDK 4.0 for body tracking. I realized that the sample codes that were published for 3.8 will not work properly on the new version. I am trying to edit the old files myself but was wondering when will the new example codes be published.
Thank you

Hello,

New example codes are published in Github. GitHub - stereolabs/zed-sdk: ⚡️The spatial perception framework for rapidly building robots and spaces that sense and understand their surroundings

You can also access new example codes in installation folder.

Hello, thank you for your support.
The initial problem seems solved, but now I face a much bigger one when running the file. My whole PC start shutting down and I get the blue screen of windows. It might be related to multithreading.
The error I got was the following:

Stop code: SYSTEM_THREAD EXCEPTION_NOT_HANDLED
What failed: nvlddmkm.sys

System info:
ZED2
OS: Windows 11 pro on ASUS Laptop.
GPUs:

  • Nvidia
  • Intel, which is integrated.

Hi,

It looks like a GPU driver crash. Can you try upgrading the driver to the latest stable version?

Best regards.

It worked now after updating my GPU driver, thanks :smiley: :+1:. However, it seems there is a problem in BODY_34 as it doesn’t show anything when I run it. How can we fix it ?

BODY_18 , BODY_38, and BODY_70 work fine.

Thank you,