I am struggling to get the sdk to work.
I get this error-message:
File “c:\Users\70550305\OneDrive\3d\python\zed\tutorial_zed.py”, line 21, in
import pyzed.sl as sl
ImportError: DLL load failed while importing sl: The specified module could not be found.
I have done the following:
- installing SDK
- Creating an environment in Anaconda
- opening a terminal from the environment - running the get_python_api.py script
- Checking that the pyzed package is installed.
- Launching a script from the same enivronment
I have tried both the sdk 3 and 4, and also with different python version, but now i do not have any more ideas. I see that more people have this problem, but their solution of copying files has not worked for me. I have also tried to downgrade python to 3.6
Any help is appreciated ![]()