Power issue with ORIN NX 16GB

Hello,

I’m having an issue with the power supply of my ORIN NX 16GB. When I plug in the power cable, the Zedbox doesn’t always start automatically. It looks like there’s a loose connection.

What would you recommend I do?

Hi @twensta
We do not recommend unplugging and replugging the power cable, but to keeping it screwed to the front panel.
The better practice is to unplug a replug the wall power cord.

I understand, however I also experience issues when I unplug and replug the wall power cord.

Are you facing this kind of problem for cold boot or hot boot?
I mean, only if you power the device after it has stayed off for many hours, or only if you turn it off and on consecutively?

I ran some tests today, and the results are quite random. The first plug-in of the day boots immediately. However, after that, the behavior becomes inconsistent: sometimes it reboots right away, and sometimes it doesn’t reboot even after waiting 1 or 2 minutes with the cable unplugged.

This Jetson will be used on an autonomous boat, so such behavior could be really problematic.

I’m also unable to perform a reboot from the command line. The Jetson simply shuts down and never reboots.

Please write an email to support@stereolabs.com with a link to this thread.