Possible use of 3rd Party Cameras (with or w/o GMSL2))

Hi, we have the requirement to use a special 100° FOV rectilinear photogrammetry lens with C-Mount and 14mm image circle (= 1” sensor format), so we would like to use a 3rd party camera. Our goal is realtime coverage mapping but also later a 360 point cloud. We use triggered LED lighting.

  1. We already run our own IMX530 hardware triggered OrinNX based camera system which we would prefer if it could stream data directly, but could also use e.g. a Leopard Imaging GSML2 camera instead of our system. Do I understand the 3rd-party devices site correctly that this would be possible, and if so, what are the steps?
  2. We are not trying to bypass stereolabs hardware but would ideally mix several of our 1” mapping cameras with further ZED X One S fisheye units for surround perception. Would this be possible, too?

Thanks so much in advance!

Tom

Hi @360vision
Welcome to the Stereolabs community.

Please add details on the final configuration you want to achieve so I can provide all the relevant information.

I have sent a PM since not all relevant info is public domain. In short, it is a project that will add SLAM, situational awareness and photogrammetric mapping to a tethered underwater remotely operated vehicle (ROV).

@360vision please send instead an email to support@stereolabs.com with the same information.
This will be useful to not miss all the messages and information.