Hello everyone,
I recently brought the 4 Port PCIe USB 3.0 Card w/ 4 Channels - USB 3.0 Cards | StarTech.com Japan ](4 Port PCIe USB 3.0 Card w/ 4 Channels - USB 3.0 Cards | StarTech.com Japan), as per the recommendation to solve the problem of bandwidth.
My target is to connect 4 cameras to Jetson Xavier or Orin to get 1080@15 along with Ultra point clouds.
After connecting everything, I am still getting errors for another two cameras as not found. I found out that it might be because of the power supply. As currently card is not using any external power supply Through SATA or LP4.
Here I was wondering if someone has achieved without using an external power supply. Or if power is needed, what are possible ways I can do it?
Thank you so much!
My lsusb on orin looks like
/: Bus 10.Port 1: Dev 1, Class=root_hub, Driver=xhci_hcd/1p, 5000M
|__ Port 1: Dev 2, If 0, Class=Video, Driver=uvcvideo, 5000M
|__ Port 1: Dev 2, If 1, Class=Video, Driver=uvcvideo, 5000M
/: Bus 09.Port 1: Dev 1, Class=root_hub, Driver=xhci_hcd/1p, 480M
|__ Port 1: Dev 2, If 0, Class=Human Interface Device, Driver=usbhid, 12M
/: Bus 08.Port 1: Dev 1, Class=root_hub, Driver=xhci_hcd/1p, 5000M
|__ Port 1: Dev 2, If 0, Class=Video, Driver=uvcvideo, 5000M
|__ Port 1: Dev 2, If 1, Class=Video, Driver=uvcvideo, 5000M
/: Bus 07.Port 1: Dev 1, Class=root_hub, Driver=xhci_hcd/1p, 480M
|__ Port 1: Dev 2, If 0, Class=Human Interface Device, Driver=usbhid, 12M
/: Bus 06.Port 1: Dev 1, Class=root_hub, Driver=xhci_hcd/1p, 5000M
|__ Port 1: Dev 2, If 0, Class=Video, Driver=uvcvideo, 5000M
|__ Port 1: Dev 2, If 1, Class=Video, Driver=uvcvideo, 5000M
/: Bus 05.Port 1: Dev 1, Class=root_hub, Driver=xhci_hcd/1p, 480M
|__ Port 1: Dev 2, If 0, Class=Human Interface Device, Driver=, 12M
/: Bus 04.Port 1: Dev 1, Class=root_hub, Driver=xhci_hcd/1p, 5000M
|__ Port 1: Dev 2, If 0, Class=Video, Driver=uvcvideo, 5000M
|__ Port 1: Dev 2, If 1, Class=Video, Driver=uvcvideo, 5000M
/: Bus 03.Port 1: Dev 1, Class=root_hub, Driver=xhci_hcd/1p, 480M
|__ Port 1: Dev 2, If 0, Class=Human Interface Device, Driver=usbhid, 12M
/: Bus 02.Port 1: Dev 1, Class=root_hub, Driver=tegra-xusb/4p, 10000M
|__ Port 3: Dev 2, If 0, Class=Hub, Driver=hub/4p, 10000M
/: Bus 01.Port 1: Dev 1, Class=root_hub, Driver=tegra-xusb/4p, 480M
|__ Port 3: Dev 2, If 0, Class=Wireless, Driver=rtk_btusb, 12M
|__ Port 3: Dev 2, If 1, Class=Wireless, Driver=rtk_btusb, 12M
|__ Port 4: Dev 3, If 0, Class=Hub, Driver=hub/4p, 480M
|__ Port 1: Dev 4, If 0, Class=Human Interface Device, Driver=usbhid, 1.5M
|__ Port 2: Dev 5, If 0, Class=Human Interface Device, Driver=usbhid, 1.5M