We have 6 ZED cameras performing fusion. Accurate, non-glitchy skeleton data (of type BODY 38) is very important for our use case. Running the following settings in the “Edge Body Tracking” application through ZED hub yields an average camera FPS of about 8-9 when running ZED 360:
I understand that high FPS is of importance, particularly during calibration, and I believe our achieved FPS is quite low. What are your advice for the optimal settings to use in order to maximize the FPS achieved during calibration, and more importantly, when recording skeleton data?