I’m currently trying to set up the zed_multi.urdf.xacro method with multiple cameras (1 stereo, 2 mono).
What are the optical origins of the ZedX and ZedXOne GS to position them in the reference frame?
I’m currently trying to set up the zed_multi.urdf.xacro method with multiple cameras (1 stereo, 2 mono).
What are the optical origins of the ZedX and ZedXOne GS to position them in the reference frame?
Hi @d1324
you can extract this information from the xacro files of the ZED ROS 2 Wrapper:
@Myzhar Thank you. So define the camera relations based on each ¼-20" threaded screw hole?
Looks like the reference point of the zedx is the center of camera between the eyes and not the left eye correct?
Yes, this is correct when using ROS and ROS 2.