I want to purchase a ZED X mini, but I don’t know if it can function properly in my working environment. The required operating temperature is 0 to 50°C, with operating and storage humidity of 10% to 85%, and a storage temperature of -20 to 60°C.
Hi @Qian
Welcome to the StereoLabs community.
The declared operative range of the ZED X Mini (see datasheet) is -20°C to +55°C.
The camera can be safely stored with a temperature between -20°C and 60°C.
We do not have data concerning the humidity range. In any case, the camera is IP67 rated.