I am trying to run the object detection image viewer sample included with the installation of the SDK.
The first time i tried to run it it didn’t find the OpenGL module, so I installed it with pip.
After this, I got the following error:
OpenGL.error.Error: Attempt to retrieve context when no valid context
What am I missing?
Thank you all in advance!
Edit:
This is the whole output, it shows a cuDNN error too…
(venv1) martin@martin-ubuntu:~/Desktop/python$ python3 object_detection_image_viewer.py --input_svo_file filare.svo2
}[Sample] Using SVO File input: filare.svo2
[Sample] Using default resolution
[2024-12-11 11:14:08 UTC][ZED][INFO] Logging level INFO
[2024-12-11 11:14:08 UTC][ZED][INFO] Logging level INFO
[2024-12-11 11:14:08 UTC][ZED][INFO] Logging level INFO
[2024-12-11 11:14:10 UTC][ZED][INFO] [Init] Depth mode: PERFORMANCE
[2024-12-11 11:14:10 UTC][ZED][INFO] [Init] Serial Number: S/N 26962166
[2024-12-11 11:14:11 UTC][ZED][ERROR] [Object Detection] cuDNN library not found
[2024-12-11 11:14:11 UTC][ZED][ERROR] [ZED] [Object Detection] CUDNN NOT FOUND
[2024-12-11 11:14:11 UTC][ZED][WARNING] CORRUPTED SDK INSTALLATION in sl::ERROR_CODE sl:
:enableObjectDetection(sl::ObjectDetectionParameters)
Traceback (most recent call last):
File “/home/martin/Desktop/python/object_detection_image_viewer.py”, line 145, in
main()
^^^^^^
File “/home/martin/Desktop/python/object_detection_image_viewer.py”, line 102, in main
viewer.init(camera_info.camera_configuration.calibration_parameters.left_cam, obj_param.enable_tracking)
File “/home/martin/Desktop/python/ogl_viewer/viewer.py”, line 549, in init
glutDisplayFunc(self.draw_callback)
File “/home/martin/directory_env/venv1/lib/python3.12/site-packages/OpenGL/GLUT/special.py”, line 147, in call
contextdata.setValue( self.CONTEXT_DATA_KEY, cCallback )
File “/home/martin/directory_env/venv1/lib/python3.12/site-packages/OpenGL/contextdata.py”, line 58, in setValue
context = getContext( context )
^^^^^^^^^^^^^^^^^^^^^
File “/home/martin/directory_env/venv1/lib/python3.12/site-packages/OpenGL/contextdata.py”, line 40, in getContext
raise error.Error(
OpenGL.error.Error: Attempt to retrieve context when no valid context