Hi everyone,
I am posting here hoping to find clarification regarding an issue I am experiencing since a few months, quite annoying and up to now without a traceable cause. It happens at random but when it does it is quite destructive.
PROBLEM DESCRIPTION
Camera is working fine with positional tracking, depth, sensors being sampled correctly by a software I wrote accoring to your documentation and sl/Camera.hpp; after some time it randomly fails with these symptoms:
- grab() returns ERROR CAMERA_REBOOTING;
- the nvargus error messages reported below appear in the console log;
- camera has to be restarted to become usable again, i.e. my software has to be forcibly terminated then re-started to re-open the camera which then works fine again.
NVARGUS ERROR MESSAGES
Just an excerpt that I was able to extract.
(Argus) Error Timeout: (propagating from src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 137)
(Argus) Error Timeout: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
(Argus) Error FileOperationFailed: Failed socket read: Connection reset by peer (in src/rpc/socket/common/SocketUtils.cpp, function readSocket(), line 79)
(Argus) Error FileOperationFailed: Unexpected error in reading socket (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 277)
(Argus) Error FileOperationFailed: Receive worker failure, notifying 2 waiting threads (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 350)
(Argus) Error InvalidState: Argus client is exiting with 2 outstanding client threads (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 366)
(Argus) Error FileOperationFailed: Receiving thread terminated with error (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadWrapper(), line 379)
(Argus) Error FileOperationFailed: Client thread received an error from socket (in src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 145)
(Argus) Error FileOperationFailed: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
SETUP DESCRIPTION
- Nvidia Jetson Orin NX 16GB (custom carrier)
- ZED Link Mono capture card connected to CSI port on Orin, 9 V power supplied from battery
- JetPack 6.2.1 (full installation by Nvidia SDKManager)
- ZED X/X Mini camera (tested with both, happens with both)
- ZED Link driver 1.3.1 (correctly installed from
.debpackage) - ZED SDK 5.0.3
- Software written in C++ using ZED SDK, running inside a Docker container set up following your documentation (full privileges, udev rules installed on the host,
systemdservice volume mounted etc.) - Running positional tracking, resolution
HD1200,NEURAL_LIGHTdepth mode, IMU sampling
Many thanks to everyone who is willing to help,
RM