Hello,
We had recently purchased 4 ZED X1 GS 4mm cameras and ZED Box Orin NX alongside with GMSL support as well. The setup was done by following this link : Get Started with ZED X One - Stereolabs. After setting up the nvargus and the zedx-one-capture to stream image data out, we are able to see just 2 camera streams at a time even when all 4 cameras are connected. Looking into the troubleshooting guide, we also set the speed of the MIPI lanes by following the same instructions. Please let us know how to ensure we can stream from all 4 cameras at a time