Hello,
using zed_ros_wrapper i am facing the following error:
[ INFO] [1676074440.766349484]: *** Opening ZED 2...
[ INFO] [1676074443.997528502]: ZED connection -> NO GPU COMPATIBLE
If i go to /usr/local/zed/tools and run the apps camera is working properly. I also did Zed_diagnostic and everything was fine.
my gpu is geforce 940MX
Graphics Features
DirectX
12 (11_0)
OpenGL
4.6
OpenCL
3.0
Vulkan
1.3
CUDA
5.0
Shader Model
6.7 (5.1)
i also run the following command
geo@geo:~/catkin_ws$ nvidia-smi --query-gpu=compute_cap --format=csv
compute_cap
5.0
nvidia-smi
Sun Feb 12 00:27:47 2023
+-----------------------------------------------------------------------------+
| NVIDIA-SMI 515.43.04 Driver Version: 515.43.04 CUDA Version: 11.7 |
I dont know if its something simple, but any help would be appreciated!!
my OS is 18.04 LTS
ZED SDK 3.8.2. On ZED SDK 3.7 i dont have this problem.
Thanks in advance!!