Copying from: No calibration file found for SN XXX. Downloading... runs forever · Issue #726 · stereolabs/zed-sdk · GitHub
Preliminary Checks
-
This issue is not a duplicate. Before opening a new issue, please search existing issues.
This issue is not a question, feature request, or anything other than a bug report directly related to this project.
Description
When I run:
init_params.set_from_svo_file(svo_file)
err = zed.open(init_params)
it outputs:
[2025-10-01 05:02:59 UTC][ZED][INFO] Logging level INFO
[2025-10-01 05:02:59 UTC][ZED][INFO] [Init] Depth mode: NONE
[2025-10-01 05:02:59 UTC][ZED][INFO] [Init] Serial Number: S/N 17225336
[2025-10-01 05:02:59 UTC][ZED][INFO] [Init] No calibration file found for SN 17225336. Downloading...
it then gets stuck here and runs forever. I wonder why is it so slow? My network is actually pretty good. I tried using the command line to download from the website as wget -O SN17225336.conf "http://calib.stereolabs.com/?SN=17225336" which is fast.
Steps to Reproduce
init_params.set_from_svo_file(svo_file)
err = zed.open(init_params)
Expected Result
fast calibration file download.
Actual Result
[2025-10-01 05:02:59 UTC][ZED][INFO] Logging level INFO
[2025-10-01 05:02:59 UTC][ZED][INFO] [Init] Depth mode: NONE
[2025-10-01 05:02:59 UTC][ZED][INFO] [Init] Serial Number: S/N 17225336
[2025-10-01 05:02:59 UTC][ZED][INFO] [Init] No calibration file found for SN 17225336. Downloading…
ZED Camera model
ZED
Environment
docker container built based on `nvidia/cuda:12.4.1-cudnn-devel-ubuntu22.04`
Environment (mine)
Ubuntu 22.04, Zed SDK 22.04
For me, I fixed the Zed X this way by manually downloading the calibration file according to Download Calibration File , however it doesn’t work for opening the CameraOne.
I suspect this has something to do with Zed 5.0.7 fix
- Fixed a
TypeErrorwhen callingget_camera_informationfrom a ZEDOne with the Python API.