Jetson Orin AGX
SDK 3.8.2 (Yesterdays Download) 2023-02-06T00:00:00Z
Ubuntu 20.04.5 LTS
I don’t have my camera yet (Zed X) so I’m trying to learn on sample data. Got the SDK installed along with python api and everything else as far as I know. I’m new so it’s all a learning curve. This is the code I used altered from
Using the Video API | Stereolabs
https://support.stereolabs.com/hc/en-us/articles/1500009269601-Are-there-any-video-image-samples-from-the-ZED-products-that-I-can-see-and-test-before-the-purchase-
import sys
from sys import exit
import pyzed.sl as sl
# Create a Zed Camera object.
zed = sl.Camera()
# Set SVO path for playback.
# "/home/j/Downloads/ZED2_HD2K_Runners_H264.svo"
# input_path = sys.argv[1]
init_parameters = sl.InitParameters()
init_parameters.set_from_svo_file("/home/j/Downloads/ZED2_HD2K_Runners_H264.svo")
# Open the Zed
zed = sl.Camera()
err = zed.open(init_parameters)
svo_image = sl.Mat()
while not sys.exit:
if zed.grab() == sl.ERROR_CODE.SUCCESS:
# Read side by side frames stored in the SVO
zed.retrieve_image(svo_image, sl.VIEW.SIDE_BY_SIDE)
# Get frame count
svo_position = zed.get_svo_position();
elif zed.grab() == sl.ERROR_CODE.END_OF_SVOFILE_REACHED:
print("SVO end has been reached. Looping back to first frame")
zed.set_svo_position(0)
exit()
if I run, after chmoding the file, as
python3 “SVO_Tutorial_One.py” ZED2_HD2K_Runners_H264.svo
Output is this: I have no idea where to look these codes up yet. Any help would be appreciated.
Opening in BLOCKING MODE
NvMMLiteOpen : Block : BlockType = 261
NVMEDIA: Reading vendor.tegra.display-size : status: 6
NvMMLiteBlockCreate : Block : BlockType = 261
Opening in BLOCKING MODE
NvMMLiteOpen : Block : BlockType = 261
NVMEDIA: Reading vendor.tegra.display-size : status: 6
NvMMLiteBlockCreate : Block : BlockType = 261
Thanks for your time,
Jay.