New SDK 5.3.0 camera disconnect within hour

testsystem: jetson AGX ORIN

stereolabs duo camera with V1.4.1 driver

sdk 5.3.0 with 3x ZEDX camera attached

camera’s and computer are fixed positioned on a desk without any viberation or touch.

within an hour with testing with the new V5.3.0 sdk we get the following error:

[2026-05-11 10:00:46 UTC][ZED][ERROR] [ZED-Argus][CAM2] Camera configuration error detected, this may be due to a flaky connection or power issue. Please check the physical connections.
[2026-05-11 10:00:46 UTC][ZED][ERROR] [ZED] GMSL camera detected as disconnected. Please do not remove GMSL cameras at runtime or inspect for damage and/or loose connections. You may need to restart the zed_x_daemon: sudo systemctl restart zed_x_daemon.service or perform a full system reboot.
can’t readout image: 0Result: CAMERA NOT DETECTED

with the older sdk 5.1.1 the same software worked for days without any issue. (we revert the sdk and let it run again without any issue).

Is this a known issue for the new sdk?

Hi @Martijn
please add more details, mostly regarding the multi-camera setup, the processing type, the depth mode, etc.

A GMSL2 report would also be useful: sudo ZED_Diagnostic --dmesg.

after some more testing, it seems some cabling issue. problem solved now