Good afternoon!
I have one ZED Box Orin and four ZED X cameras connected via GMSL2. All cameras are connected to a single box. I’m a bit confused. Based on the example in the recording_multi.py file, it seems like the cameras are initialized sequentially, not simultaneously in a synchronized manner.
Since I have one ZED Box with four cameras connected, do I still need to set up the PTP Service to synchronize the devices, as described here? Cause I have such output
$ nmcli device status
DEVICE         TYPE      STATE                   CONNECTION
eth0           ethernet  connected               Wired connection 1
l4tbr0         bridge    connected (externally)  l4tbr0
wlan0          wifi      disconnected            –
p2p-dev-wlan0  wifi-p2p  disconnected            –
can0           can       unmanaged               –
usb0           ethernet  unmanaged               –
usb1           ethernet  unmanaged               –
lo             loopback  unmanaged               –
$ ethtool -T eth0
Time stamping parameters for eth0:
Capabilities:
software-transmit
software-receive
software-system-clock
PTP Hardware Clock: none
Hardware Transmit Timestamp Modes: none
Hardware Receive Filter Modes: none
So, do I need to use “software mode”?
Also, I would like to clarify the following: based on recording_multi.py, each camera is opened one after another, with a slight delay.
Is there a way to wait until all cameras are opened and then start recording on all of them at the same time?
Can this be achieved through code, or does it require some additional setup?
— UPD —
ZED Link Driver is updated to 1.3.1 as I noticed, there’s a point saying “Support camera synchronization for precise multi-camera capture.”
My question is: does this happen automatically?
For more detailed info, I’m using a ZED Link Duo capture card with four ZED X cameras connected to a ZED Box Orin 8GB.
Best regards,
Ed Ti