Multicamera setup

Hi @zekanysz, sorry for the delay.

  • I can make an SVO recording for sure. What should I do only start the github example and save it in an svo file? Or should I stand in front of the camera within 1.3 meter or position the doll or box or something in front of the camera?

Yes, that’s it. Show the problematic situation, so start from the range you need, then the range where the detection starts. We’ll concentrate on why is doesn’t work under this. You can record it using ZED Explorer, it’s easier than the sample, just enable the “H265 LOSSY” or “H264 LOSSY” if 265 is not available in the “General” tab of the settings.

Should we use the ZED i cameras or is the ZED 2 cameras perfect too?

I advise going for the ZED 2i, they are much more reliable (better enclosure) and use an external USB connection, avoiding rare but very difficult-to-fix USB issues.

“No module named ‘pyzed.sl’

  • Which Python version are you using?
  • Do you use a virtual environment like conda?
  • Does the get_python_api.py give out any errors when you run it?