The fusion in the new ZED SDK 4.1 seems to be missing all the fused Object Detection.
I install the latest version of the ZED SDK 4.1
I started to build the Multi-Camera Object Detection sample and I Get Errors:
class “sl::Fusion” has no member “enableObjectDetection”.
class "sl::Fusion: has no member “retrieveObjects”.
I did find Class ObjectDetectionFusionParameters .
I went into the fusion Header file in the ZED SDK 4.1 and Looked for them to see maybe I was pathing anything wrong but there is no methods that match these or anything on enabling multi cam object detection.
Please let me know if I need to grab another update for the ZED SDK
Thanks!