when I modify the parameters by code the result does not change as on the software one has a result of contour!
Hi @Sabrina
Welcome to the Stereolabs community.
Can you post the source code you used?
Thank you for your reply.
In my code i introduce by this two function :
def set_runtimeParameters(self,sensing_mode=sl.SENSING_MODE.STANDARD):
self.runtime_params = sl.RuntimeParameters()
self.runtime_params.sensing_mode = sensing_mode
def set_confidence_params(self,confidence_threshold = 100, textureness_confidence_threshold=81):
self.runtime_params.confidence_threshold = confidence_threshold
self.runtime_params.textureness_confidence_threshold = textureness_confidence_threshold
and the result :
Can you please write an email to support@stereolabs.com sharing the SVO file that you are using so we can test it?