Measuring Surface Roughness Using the ZED 2i Camera

Hello Team

I am currently working on a project where I need to analyze the roughness of various surfaces, such as roads or pavement. Surface roughness refers to the irregularities or variations in height at different points of a surface, typically measured by the variations in the surface’s texture or depth over a given area. The goal is to capture these variations accurately to assess factors like wear, tear, and degradation.

I’m considering using the ZED 2i camera for this task, specifically leveraging its depth-sensing capabilities to detect small irregularities and variations in the surface. I would like to know if the ZED 2i camera is suitable for measuring surface roughness, and if so, what specific techniques or SDK features I should use to obtain precise roughness measurements.

Are there any depth post-processing methods or filtering options that would help improve the detection of small surface irregularities? I’m also interested in whether using normal map extraction or other methods could enhance the accuracy of roughness quantification.

Any insights or recommendations for measuring surface roughness with the ZED 2i would be greatly appreciated!

Thank you in advance!

Hi @karthikreddy157
what is the depth difference range that you must measure?
What depth accuracy/resolution do you need?

Hi @Myzhar ,
The camera will be mounted at 1 to 1.5 meters(possible to adjust for better precision) high at the start point, the difference range will around 0.1 to 50 millimeters

Thank you.

Hi @karthikreddy157
the ZED 2i can work in this type of condition, but only if the vehicle is moving slowly; otherwise, you will get blurred information.
For high speed we recommend the ZED X camera models with Global Shutter CMOS sensors.

Can define slowly (in km/hr)

I can’t because it depends on many factors:

  • distance
  • angle
  • FPS
  • exposure time
  • etc

I have a similar problem; I need to scan an area ahead of the user, who wears the ZED2I at hip height in front, to scan an area between 1.5 and 3.5 meters ahead, while walking, and scan for path irregularities that could trip the user, so hope to detect the Floor and trip hazards as low as 3-5 mm… is this possible. I have spekt 2 days with chatgpt 5.4, extended thinking, getting nowhere…

This is out of the capability of the ZED 2i camera.
The accuracy in the range [1.5,3.5] m is about 1%, so +/- 0.015 m and +/-0.035 m