Jetson Orin Nx Zed x one

Hello,

I recently bought two ZED X ones and flashed my Jetson Orin NX (SEEED reComputer J4012-Edge NVIDIA Jetson Orin™ NX 16GB). I successfully flashed my Jetson with L4T 36.4.3 and Jetpack 6.2 (rev 1), and when I tried to open my two zed x one with the ZED Media Server, I have this error:

ZED_Media_Server

[ZEDMediaServer] Version 0.1.9

[ZEDMediaServer] Stopping Media Server service…

[sudo] password for jetson:

…done

[ZEDMediaServer] Found: 2 available cameras

[ZEDMediaServer] Opening camera 0 at Resolution 1920 x 1080 @ 15

[ZXCamera] Setup State error: 10

[ZEDMediaServer] Failed to open camera 0 at resolution 1920 x 1080 @ 15 ==> ErrCode= 10

[ZEDMediaServer] Opening camera 1 at Resolution 1920 x 1080 @ 15

bmi08g_init Error [-2]: Communication failure

bmi08g_set_int_config Error [-2]: Communication failure

[ZXCamera] Setup State error: 2

[ZEDMediaServer] Failed to open camera 1 at resolution 1920 x 1080 @ 15 ==> ErrCode= 2
dmesg.log (27.6 KB)
Thanks

Hi @LucasMarchnd
Seeed Studio devices are not compatible with our GMSL2 products