Jetson AGX Orin 64GB sdk installation

Hi,
Just got a brand new Jetson ZED Box and I am trying to install the SDK on ir but it does not work.
I get this message when running the installer :
Verifying archive integrity… 100% MD5 checksums are OK. All good.
Uncompressing ‘ZED camera SDK by Stereolabs (Use ‘sudo apt install zstd’ if zstd is not found)’./ZED_SDK_Tegra_L4T35.3_v4.1.2.zstd.run: 1: eval: zstd: not found
… Decompression failed.
… Extraction failed.
100% Signal caught, cleaning up

It worked just fine on our Orin NX but cannot make it work on the dev kit AXG Orin

Hi @Aleblanc
as the error message says:
Use sudo apt install zstd if zstd is not found :wink:

Doesn’t work, that’s why I am asking

What does not work?
What’s the output of the command sudo apt install zstd?

Hi,

The ouput is : I am a liar!!
Apparently you need to use the command properly…

Sorry about that

The important is to solve the issue :+1: