IsaacSim Crashing with the ZED Camera Extension

Hello-

We’re doing some work evaluating the ZED cameras in simulation but running into an issue with the IsaacSim 4.5 crashing with the ZED extension installed on Windows 11.

We followed the tutorial in the documentation to the tee but the issue occurs every time we start a simulation.

Doesn’t appear to be a GPU issue since we are running a really simple simulation, IsaacSim indicates we have more than enough bandwidth, and we have meet the IsaacSim GPU requirements.

Let me know if there’s any thoughts on possible solutions.


Note: Here are some warnings I see in the IsaacSim console after starting a simulation.

2025-06-25 16:30:20 [Warning] [omni.timeline.plugin] Deprecated: direct use of ITimeline callbacks is deprecated. Use ITimeline::getTimeline (Python: omni.timeline.get_timeline_interface) instead.
2025-06-25 16:30:20 [Warning] [omni.graph.tools._impl.deprecate] internal_state() is deprecated: ‘internal_state’ has been deprecated: use ‘per_instance_state’ or ‘shared_state’
2025-06-25 16:30:20 [Warning] [omni.graph.tools._impl.deprecate] File “c:\users\owner\appdata\local\ov\data\kit\isaac-sim full\4.5\exts\3\sl.sensor.camera-3.0.0+106.5.wx64.lx64.r.cp310\sl\sensor\camera\ogn\SlCameraStreamerDatabase.py”, line 233, in compute
2025-06-25 16:30:20 [Warning] [omni.graph.tools._impl.deprecate] return SlCameraStreamerDatabase.NODE_TYPE_CLASS.compute(db)
2025-06-25 16:30:20 [Warning] [omni.graph.tools._impl.deprecate] File “c:\users\owner\appdata\local\ov\data\kit\isaac-sim full\4.5\exts\3\sl.sensor.camera-3.0.0+106.5.wx64.lx64.r.cp310\sl\sensor\camera\ogn\nodes\SlCameraStreamer.py”, line 287, in compute
2025-06-25 16:30:20 [Warning] [omni.graph.tools._impl.deprecate] SlCameraStreamer.createStreamer(db)
2025-06-25 16:30:20 [Warning] [omni.graph.tools._impl.deprecate] File “c:\users\owner\appdata\local\ov\data\kit\isaac-sim full\4.5\exts\3\sl.sensor.camera-3.0.0+106.5.wx64.lx64.r.cp310\sl\sensor\camera\ogn\nodes\SlCameraStreamer.py”, line 191, in createStreamer
2025-06-25 16:30:20 [Warning] [omni.graph.tools._impl.deprecate] db.internal_state.imu_sensor_interface = _sensor.acquire_imu_sensor_interface()
2025-06-25 16:30:20 [Warning] [omni.graph.tools._impl.deprecate]
2025-06-25 16:30:20 [Warning] [sl.sensor.camera.ogn.nodes.SlCameraStreamer] Overriding simulation time by system time

Hi, could you run a diagnostic using the ZED Diagnostic tool installed with the ZED SDK and share the report?

Ben-

Please the the diagnostics output below.


{
“AI Models”: {
“info”: [
“MULTI CLASS DETECTION is not optimized”,
“MULTI CLASS MEDIUM DETECTION is not optimized”,
“MULTI CLASS ACCURATE DETECTION is not optimized”,
“HUMAN BODY FAST DETECTION is not optimized”,
“HUMAN BODY MEDIUM DETECTION is not optimized”,
“HUMAN BODY ACCURATE DETECTION is not optimized”,
“HUMAN BODY 38 FAST DETECTION is not optimized”,
“HUMAN BODY 38 MEDIUM DETECTION is not optimized”,
“HUMAN BODY 38 ACCURATE DETECTION is not optimized”,
“PERSON HEAD DETECTION is not optimized”,
“PERSON HEAD ACCURATE DETECTION is not optimized”,
“REID ASSOCIATION is not optimized”,
“NEURAL PLUS DEPTH is not optimized”
],
“valid”: [
“NEURAL LIGHT DEPTH is optimized”,
“NEURAL DEPTH is optimized”
]
},
“Camera Test”: {
“InternalDevicesCount (GMSL)”: 0,
“InternalDevicesCount (USB)”: 0,
“ZEDCount”: 0,
“ZEDs”: [
],
“error”: [
“Camera not detected
Make sure the camera is plugged in or try another USB 3.0 port.”
]
},
“Devices”: {
“ASMediaFound”: false,
“CorruptedFirmware”: false,
“OC_Cam_Detected”: false,
“OtherUSBDevices”: [
],
“USBList”: [
{
“USB_path”: “/5”,
“idProduct”: “0x101d”,
“idVendor”: “0x05ac”
},
{
“USB_path”: “/10”,
“idProduct”: “0x0033”,
“idVendor”: “0x8087”
},
{
“USB_path”: “/1/4”,
“idProduct”: “0x1114”,
“idVendor”: “0x05ac”
},
{
“USB_path”: “/5/4”,
“idProduct”: “0x1114”,
“idVendor”: “0x05ac”
},
{
“USB_path”: “/7”,
“idProduct”: “0x0051”,
“idVendor”: “0x3277”
},
{
“USB_path”: “/1”,
“idProduct”: “0x101d”,
“idVendor”: “0x05ac”
},
{
“USB_path”: “/5/4”,
“idProduct”: “0x1114”,
“idVendor”: “0x05ac”
},
{
“USB_path”: “/8”,
“idProduct”: “0x193b”,
“idVendor”: “0x0b05”
},
{
“USB_path”: “/6”,
“idProduct”: “0x19b6”,
“idVendor”: “0x0b05”
},
{
“USB_path”: “/3”,
“idProduct”: “0x101e”,
“idVendor”: “0x05ac”
}
],
“ZEDDetected”: null,
“captureDevices”: [
],
“controllers”: [
{
“CompatibleIDs”: “USB\USB20_HUB”,
“Description”: “Generic USB Hub”,
“DeviceName”: “”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0014”,
“Location”: “Port_#0005.Hub_#0005”,
“Manufacturer”: “(Standard USB HUBs)”,
“Name”: “USB”,
“PhysicalName”: “\Device\USBPDO-6”
},
{
“CompatibleIDs”: “PCI\VEN_8086&DEV_7E7D&REV_20”,
“Description”: “USB xHCI Compliant Host Controller”,
“DeviceName”: “Intel(R) USB 3.20 eXtensible Host Controller - 1.20 (Microsoft)”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0002”,
“Location”: “PCI bus 0, device 20, function 0”,
“Manufacturer”: “Generic USB xHCI Host Controller”,
“Name”: “PCI”,
“PhysicalName”: “\Device\NTPNP_PCI0012”
},
{
“CompatibleIDs”: “”,
“Description”: “USB Root Hub (USB 3.0)”,
“DeviceName”: “”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0004”,
“Location”: “”,
“Manufacturer”: “(Standard USB HUBs)”,
“Name”: “USB”,
“PhysicalName”: “\Device\USBPDO-5”
},
{
“CompatibleIDs”: “PCI\VEN_8086&DEV_7EC0&REV_10”,
“Description”: “USB xHCI Compliant Host Controller”,
“DeviceName”: “Intel(R) USB 3.20 eXtensible Host Controller - 1.20 (Microsoft)”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0000”,
“Location”: “PCI bus 0, device 13, function 0”,
“Manufacturer”: “Generic USB xHCI Host Controller”,
“Name”: “PCI”,
“PhysicalName”: “\Device\NTPNP_PCI0009”
},
{
“CompatibleIDs”: “”,
“Description”: “USB Root Hub (USB 3.0)”,
“DeviceName”: “”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0003”,
“Location”: “”,
“Manufacturer”: “(Standard USB HUBs)”,
“Name”: “USB”,
“PhysicalName”: “\Device\USBPDO-0”
},
{
“CompatibleIDs”: “PCI\VEN_8086&DEV_15F0&REV_06”,
“Description”: “USB xHCI Compliant Host Controller”,
“DeviceName”: “Intel(R) USB 3.1 eXtensible Host Controller - 1.10 (Microsoft)”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0009”,
“Location”: “PCI bus 4, device 0, function 0”,
“Manufacturer”: “Generic USB xHCI Host Controller”,
“Name”: “PCI”,
“PhysicalName”: “\Device\NTPNP_PCI0032”
},
{
“CompatibleIDs”: “”,
“Description”: “USB Root Hub (USB 3.0)”,
“DeviceName”: “”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0010”,
“Location”: “”,
“Manufacturer”: “(Standard USB HUBs)”,
“Name”: “USB”,
“PhysicalName”: “\Device\USBPDO-1”
},
{
“CompatibleIDs”: “USB\USB30_HUB”,
“Description”: “Generic SuperSpeed USB Hub”,
“DeviceName”: “”,
“Driver”: “{36fc9e60-c465-11cf-8056-444553540000}\0011”,
“Location”: “Port_#0003.Hub_#0002”,
“Manufacturer”: “(Standard USB HUBs)”,
“Name”: “USB”,
“PhysicalName”: “\Device\USBPDO-2”
}
],
“notTested”: [
“Please connect a camera to test the USB connection.”
]
},
“Graphics Card”: {
“deviceCount”: 1,
“deviceDriverVersion”: 12090,
“devices”: [
{
“arch”: “Ada Lovelace”,
“computeCapability”: “8.9”,
“cores”: 9728,
“name”: “NVIDIA GeForce RTX 4090 Laptop GPU”,
“totalMemoryBytes”: “17170956288”,
“totalMemoryMB”: 16375.5
}
],
“initResult”: 0,
“valid”: [
“Graphics card: NVIDIA GeForce RTX 4090 Laptop GPU”
]
},
“Processor”: {
“OS”: “Windows 10 FallCreators”,
“avxSupported”: true,
“coreCount”: “16”,
“cpu”: “Intel(R) Core™ Ultra 9 185H”,
“datetime”: “2025-07-07 22:43:37”,
“hyperThreading”: “1”,
“motherboard”: ", ",
“ramCapacity”: “31.4163”,
“ramUsage”: “0”,
“ramUsed”: “15.4653”,
“threadCount”: “22”,
“valid”: [
“Processor: Intel(R) Core™ Ultra 9 185H”
]
},
“ZED SDK”: {
“CUDA Toolkit version”: “V12.9.41 -->located in C:/Program Files/NVIDIA GPU Computing Toolkit/CUDA/v12.9/bin/nvcc.exe”,
“CUDA loading”: false,
“ZED SDK Version (Diag)”: “5.0.1”,
“ZED SDK Version (RT)”: “5.0.1”,
“ai”: {
“checkAI”: true,
“cudaVersion”: 12090,
“tensorVersion”: 100900
},
“binFiles”: [
“nvinfer_10.dll”,
“nvinfer_builder_resource_10.dll”,
“nvinfer_dispatch_10.dll”,
“nvinfer_lean_10.dll”,
“nvinfer_plugin_10.dll”,
“nvinfer_vc_plugin_10.dll”,
“nvonnxparser_10.dll”,
“sl_ai64.dll”,
“sl_zed64.dll”,
“zlibwapi.dll”
],
“driverVersion”: “576.02”,
“drivervDllVersion”: “32.0.15.7602”,
“resourcesFiles”: [
“neural_depth_5.2.model”,
“neural_depth_5.2.model_optimized-fbcbw-1-89-12090-100900-17-256-65536-48-100-512-76-0-0e53-512”,
“neural_depth_light_5.2.model”,
“neural_depth_light_5.2.model_optimized-fbcbw-1-89-12090-100900-17-256-65536-48-100-512-76-0-0e53-512”,
“w100900_timing_cache”
],
“resourcesFilesExpected”: [
“objects_performance_3.2”
],
“runtimeDllVersion”: 12090,
“valid”: [
“ZED SDK version: 5.0.1”,
“CUDA version: V12.9.41”
]
}
}

Hi,

I confirm the crash. This should be fixed very soon. I’ll keep you updated.

Sorry for that.

Hi,

A new version of the extension (v3.1.1) containing the fix has just been published. It should be available in Isaac Sim in the next 24 hours once the extension registry is updated.

Hey Ben,

I’m only seeing up to version 3.1.0 in the IsaacSim extension window.

Not seeing 3.1.1.

Thoughts on why that might be?

Thanks in advance,

Alex