Isaac Sim 5 crashes with ZED camera extension

Hi there,

I am using Isaac-sim-5.0 with zed camera to test my robot, I followed the tutorial, installed latest ZDK SDK and isaac extension ( GitHub - stereolabs/zed-isaac-sim: NVIDIA Isaac Sim integration for ZED SDK ). However, I have the problem of starting the simulation with ZED extension, it always crashes my simulation. My setup: ZED SDK 5.0.6, CUDA version: V12.8.93, GPU: Nvidia RTX 5080.

  • The simulation scene is tested on another PC with same config (Isaac-sim-5, ZED SDK, isaac extension), simulation can be started with no error, and I can view the point cloud from zed camera in simulation.
  • I can also start the simulation with disabled ZED isaac extension.
  • But I can not start the simulation with enabled ZED isaac extension, the log from isaac sim is following, (I cannot attach file here), Many Thanks!!

2025-09-17T10:36:44Z [196,938ms] [Warning] [carb.graphics-vulkan.plugin] aftermath reports no active shader during GPU crash
2025-09-17T10:36:44Z [196,938ms] [Error] [carb.graphics-vulkan.plugin] GPU crash is detected. Trying to write crash dump into: /root/.nvidia-omniverse/logs/Kit/Isaac-Sim Full/5.0/kit_20250917_103327-0.nv-gpudmp
2025-09-17T10:36:44Z [196,938ms] [Error] [carb.graphics-vulkan.plugin] GPU crash dump is successfully written
2025-09-17T10:36:44Z [196,951ms] [Error] [carb.graphics-vulkan.plugin] VkResult: ERROR_DEVICE_LOST
2025-09-17T10:36:44Z [196,951ms] [Error] [carb.graphics-vulkan.plugin] vkWaitForFences failed for command queue.
2025-09-17T10:36:44Z [196,951ms] [Error] [gpu.foundation.plugin] A GPU crash occurred. Exiting the application…
Reasons for the failure: a device lost, out of memory, or an unexpected bug.
2025-09-17T10:36:44Z [196,952ms] [Warning] [gpu.foundation.plugin] polling aftermath dump status …
2025-09-17T10:36:44Z [197,002ms] [Warning] [gpu.foundation.plugin] successfully waited and produced aftermath dump
2025-09-17T10:36:44Z [0ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] A crash has occurred. If a debugger should be attached, please set the ‘/crashreporter/debuggerAttachTimeoutMs’ setting to a timeout in milliseconds. This can be used to allow the crash reporter to wait for up to that long for a debugger to attach before processing or sending the crash report.
2025-09-17T10:36:44Z [45ms] [Error] [carb.crashreporter-breakpad.plugin] ‘crashreport.gui’ exited with code 127
2025-09-17T10:36:44Z [46ms] [Error] [carb.crashreporter-breakpad.plugin] [crash] Wrote dump file ‘/root/.local/share/ov/data/Kit/Isaac-Sim Full/5.0/035a3b9d-57bd-4f17-edb3aa83-3e722750.dmp’
2025-09-17T10:36:44Z [47ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] preventing upload of minidump due to user opt-out: ‘/root/.local/share/ov/data/Kit/Isaac-Sim Full/5.0/035a3b9d-57bd-4f17-edb3aa83-3e722750.dmp’
2025-09-17T10:36:44Z [49ms] [Error] [carb.crashreporter-breakpad.plugin] [crash] dump file size is 5528864 bytes, file is readable.
2025-09-17T10:36:44Z [50ms] [Fatal] [carb.crashreporter-breakpad.plugin] [crash] Crash detected in pid 3982 thread 3982
2025-09-17T10:36:44Z [51ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] Crash metadata:
2025-09-17T10:36:44Z [52ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] BuildGitlabJobID = ‘182268558’
2025-09-17T10:36:44Z [53ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] CarbSdkVersion = ‘206.4+release.9396.3c6f8191.gl’
2025-09-17T10:36:44Z [55ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] CrashTime = ‘Wed Sep 17 10:36:44 2025 GMT’
2025-09-17T10:36:44Z [56ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] DriverShaderCacheWrapper = ‘disabled’
2025-09-17T10:36:44Z [57ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] DumpId = ‘035a3b9d-57bd-4f17-edb3aa83-3e722750’
2025-09-17T10:36:44Z [58ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] LastUploadStatus = ‘0’
2025-09-17T10:36:44Z [59ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] ProductName = ‘OmniverseKit’
2025-09-17T10:36:44Z [60ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] PythonTracebackStatus = ‘‘py-spy’ successfully wrote info to ‘/root/.local/share/ov/data/Kit/Isaac-Sim Full/5.0/035a3b9d-57bd-4f17-edb3aa83-3e722750.py.txt’’
2025-09-17T10:36:44Z [61ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] RetryCount = ‘0’
2025-09-17T10:36:44Z [62ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] StartupTime = ‘1758105207’
2025-09-17T10:36:44Z [64ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] UploadSuccessful = ‘0’
2025-09-17T10:36:44Z [65ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] UptimeSeconds = ‘197’
2025-09-17T10:36:44Z [66ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] UserStory = ‘’
2025-09-17T10:36:44Z [67ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] UserStoryStatus = ‘‘crashreport.gui’ exited with code 127’
2025-09-17T10:36:44Z [68ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] Version = ‘107.3.1+production.206797.8131b85d.gl’
2025-09-17T10:36:44Z [69ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] aftermath_active_shader_count = ‘0’
2025-09-17T10:36:44Z [70ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] aftermath_enabled = ‘1’
2025-09-17T10:36:44Z [71ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] aftermath_flags = ‘3’
2025-09-17T10:36:44Z [72ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] aftermath_status = ‘auto-enabled’
2025-09-17T10:36:44Z [73ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] aftermath_version = ‘2024.1’
2025-09-17T10:36:44Z [75ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] appName = ‘Isaac-Sim Full’
2025-09-17T10:36:45Z [76ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] appState = ‘started’
2025-09-17T10:36:45Z [77ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] appVersion = ‘5.0.0’
2025-09-17T10:36:45Z [78ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] autoloadExts = ‘isaacsim.ros2.urdf-1.1.19,isaacsim.ros2.tf_viewer-2.1.21,isaacsim.ros2.sim_control-1.1.4,isaacsim.ros2.bridge-4.9.3,sl.sensor.camera-4.0.1’
2025-09-17T10:36:45Z [79ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] buildBranch = ‘production’
2025-09-17T10:36:45Z [80ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] buildCi = ‘gl’
2025-09-17T10:36:45Z [81ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] buildConfig = ‘release’
2025-09-17T10:36:45Z [83ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] buildGitlabJobName = ‘kit-build-release-linux-x86_64’
2025-09-17T10:36:45Z [84ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] buildGitlabJobStage = ‘kit-build’
2025-09-17T10:36:45Z [85ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] buildGitlabPipelineID = ‘30713850’
2025-09-17T10:36:45Z [86ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] buildHash = ‘8131b85d’
2025-09-17T10:36:45Z [87ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] buildMajor = ‘107’
2025-09-17T10:36:45Z [88ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] buildMinor = ‘3’
2025-09-17T10:36:45Z [89ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] buildNumber = ‘206797’
2025-09-17T10:36:45Z [91ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] buildPatch = ‘1’
2025-09-17T10:36:45Z [92ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] buildVersion = ‘107.3.1’
2025-09-17T10:36:45Z [93ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] carboniteFrameworkVersion = ‘206.4+release.9396.3c6f8191.gl’
2025-09-17T10:36:45Z [94ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] carboniteSdkVersion = ‘206.4+release.9396.3c6f8191.gl’
2025-09-17T10:36:45Z [95ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] commandLine = ‘/isaac5/isaacsim/_build/linux-x86_64/release/kit/kit /isaac5/isaacsim/_build/linux-x86_64/release/apps/isaacsim.exp.full.kit --allow-root’
2025-09-17T10:36:45Z [96ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] cpuCoreLimited = ‘28’
2025-09-17T10:36:45Z [97ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] cpuId = ‘Intel64 Family 6 Model 183 Stepping 1’
2025-09-17T10:36:45Z [98ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] cpuLogicalCoresBareMetal = ‘40’
2025-09-17T10:36:45Z [99ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] cpuName = ‘Intel(R) Core™ i7-14700KF’
2025-09-17T10:36:45Z [101ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] cpuPhysicalCoresBareMetal = ‘20’
2025-09-17T10:36:45Z [102ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] cpuUsageQuota = ‘-1.000000’
2025-09-17T10:36:45Z [103ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] cpuVendor = ‘GenuineIntel’
2025-09-17T10:36:45Z [104ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] desktopOrigin = ‘(0, 0)’
2025-09-17T10:36:45Z [105ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] desktopSize = ‘3440x1440’
2025-09-17T10:36:45Z [106ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] displayCount = ‘1’
2025-09-17T10:36:45Z [108ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] displayRes_0 = ‘3440x1440x32bit@60Hz’
2025-09-17T10:36:45Z [109ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] environmentName = ‘Individual’
2025-09-17T10:36:45Z [110ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] externalBuild = ‘1’
2025-09-17T10:36:45Z [111ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] extraExts = ‘omni.kit.registry.nucleus-0.0.0,sl.sensor.camera-4.0.1,sl.sensor.camera.bridge-4.0.1’
2025-09-17T10:36:45Z [112ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] gpuCrash = ‘1’
2025-09-17T10:36:45Z [113ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] gpuDriver_0 = ‘580.65’
2025-09-17T10:36:45Z [114ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] gpuVRAM_0 = ‘17094934528’
2025-09-17T10:36:45Z [115ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] gpu_0 = ‘NVIDIA GeForce RTX 5080’
2025-09-17T10:36:45Z [116ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] kitRendererDriverVersion = ‘580.65’
2025-09-17T10:36:45Z [118ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] lastCommand = ‘CreateAttrCommand(node=?,attr_name=state:sdp_intergraph_downstream_node_handles,attr_type=?,attr_port=?,attr_default=?,attr_extended_type=?)’
2025-09-17T10:36:45Z [119ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] lastCommands = ‘ToggleExtension(ext_id=sl.sensor.camera-4.0.1,enable=False),ToggleExtension(ext_id=sl.sensor.camera.bridge-4.0.1,enable=False),ToolbarPlayButtonClicked,ToggleExtension(ext_id=sl.sensor.camera.bridge-4.0.1,enable=True),ToggleExtension(ext_id=sl.sensor.camera-4.0.1,enable=True),CreateAttrCommand(node=?,attr_name=state:sdp_intergraph_downstream_node_handles,attr_type=?,attr_port=?,attr_default=?,attr_extended_type=?),Group,CreateGraphAsNodeCommand(graph_path=/Orchestrator,node_name=Orchestrator,evaluator_name=push,is_global_graph=True,backed_by_usd=True,fc_backing_type=?,pipeline_stage=?,evaluation_mode=?,graph=?),CreateNodeCommand(graph=?,node_path=/Orchestrator/OgnReadFabricTime,node_type=omni.replicator.core.ReadFabricTime,create_usd=True),CreateAttrCommand(node=?,attr_name=state:sdp_intergraph_downstream_node_handles,attr_type=?,attr_port=?,attr_default=?,attr_extended_type=?)’
2025-09-17T10:36:45Z [120ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] lib_isaacSim_buildBranch = ‘main’
2025-09-17T10:36:45Z [121ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] lib_isaacSim_buildDate = ‘Fri Aug 15 17:34:10 2025 -0500’
2025-09-17T10:36:45Z [122ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] lib_isaacSim_buildHash = ‘07d8dd4’
2025-09-17T10:36:45Z [123ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] lib_isaacSim_buildRepo = ‘https://github.com/isaac-sim/IsaacSim.git’
2025-09-17T10:36:45Z [125ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] lib_isaacSim_buildVersion = ‘5.0.0-rc.45’
2025-09-17T10:36:45Z [126ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] lib_physx_buildBranch = ‘HEAD’
2025-09-17T10:36:45Z [127ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] lib_physx_buildDate = ‘Jul-23-2025’
2025-09-17T10:36:45Z [128ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] lib_physx_buildHash = ‘214216c’
2025-09-17T10:36:45Z [129ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] lib_physx_buildRepo = ‘gitlab-master.nvidia.com/omniverse/physics’
2025-09-17T10:36:45Z [130ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] lib_physx_buildVersion = ‘107.3.18’
2025-09-17T10:36:45Z [131ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] memoryStats = ‘(avail/total) RAM: 17.9139/31.1237GB, Swap: 8/8GB, VM: 1.71799e+10/1.71799e+10GB’
2025-09-17T10:36:45Z [133ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] nvidia-smi = ’
==============NVSMI LOG==============

Timestamp : Wed Sep 17 10:33:28 2025
Driver Version : 580.65.06
CUDA Version : 13.0

Attached GPUs : 1
GPU 00000000:01:00.0
Product Name : NVIDIA GeForce RTX 5080
Product Brand : GeForce
Product Architecture : Blackwell
Display Mode : Requested functionality has been deprecated
Display Attached : Yes
Display Active : Enabled
Persistence Mode : Disabled
Addressing Mode : HMM
MIG Mode
Current : N/A
Pending : N/A
Accounting Mode : Disabled
Accounting Mode Buffer Size : 4000
Driver Model
Current : N/A
Pending : N/A
Serial Number : 0
GPU UUID : GPU-48c397f4-89de-1a8e-a79f-a000925f069c
GPU PDI : 0xf373a0c2c1c4bd23
Minor Number : 0
VBIOS Version : 98.03.3B.80.E8
MultiGPU Board : No
Board ID : 0x100
Board Part Number : N/A
GPU Part Number : 2C02-400-A1
FRU Part Number : N/A
Platform Info
Chassis Serial Number :
Slot Number : 0
Tray Index : 0
Host ID : 1
Peer Type : Direct Connected
Module Id : 1
GPU Fabric GUID : 0x0000000000000000
Inforom Version
Image Version : G005.0000.98.01
OEM Object : 2.1
ECC Object : N/A
Power Management Object : N/A
Inforom BBX Object Flush
Latest Timestamp : N/A
Latest Duration : N/A
GPU Operation Mode
Current : N/A
Pending : N/A
GPU C2C Mode : Disabled
GPU Virtualization Mode
Virtualization Mode : None
Host VGPU Mode : N/A
vGPU Heterogeneous Mode : N/A
GPU Recovery Action : None
GSP Firmware Version : 580.65.06
IBMNPU
Relaxed Ordering Mode : N/A
PCI
Bus : 0x01
Device : 0x00
Domain : 0x0000
Base Classcode : 0x3
Sub Classcode : 0x0
Device Id : 0x2C0210DE
Bus Id : 00000000:01:00.0
Sub System Id : 0xF32110B0
GPU Link Info
PCIe Generation
Max : 5
Current : 2
Device Current : 2
Device Max : 5
Host Max : 5
Link Width
Max : 16x
Current : 16x
Bridge Chip
Type : N/A
Firmware : N/A
Replays Since Reset : 0
Replay Number Rollovers : 0
Tx Throughput : 23615 KB/s
Rx Throughput : 68306 KB/s
Atomic Caps Outbound : N/A
Atomic Caps Inbound : FETCHADD_32 FETCHADD_64 SWAP_32 SWAP_64 CAS_32 CAS_64
Fan Speed : 0 %
Performance State : P5
Clocks Event Reasons
Idle : Not Active
Applications Clocks Setting : Not Active
SW Power Cap : Not Active
HW Slowdown : Not Active
HW Thermal Slowdown : Not Active
HW Power Brake Slowdown : Not Active
Sync Boost : Not Active
SW Thermal Slowdown : Not Active
Display Clock Setting : Not Active
Clocks Event Reasons Counters
SW Power Capping : 467614602 us
Sync Boost : 0 us
SW Thermal Slowdown : 0 us
HW Thermal Slowdown : 0 us
HW Power Braking : 0 us
Sparse Operation Mode : N/A
FB Memory Usage
Total : 16303 MiB
Reserved : 486 MiB
Used : 613 MiB
Free : 15206 MiB
BAR1 Memory Usage
Total : 16384 MiB
Used : 36 MiB
Free : 16348 MiB
Conf Compute Protected Memory Usage
Total : 0 MiB
Used : 0 MiB
Free : 0 MiB
Compute Mode : Default
Utilization
GPU : 5 %
Memory : 9 %
Encoder : 0 %
Decoder : 0 %
JPEG : 0 %
OFA : 0 %
Encoder Stats
Active Sessions : 0
Average FPS : 0
Average Latency : 0
FBC Stats
Active Sessions : 0
Average FPS : 0
Average Latency : 0
DRAM Encryption Mode
Current : Disabled
Pending : Disabled
ECC Mode
Current : N/A
Pending : N/A
ECC Errors
Volatile
SRAM Correctable : N/A
SRAM Uncorrectable Parity : N/A
SRAM Uncorrectable SEC-DED : N/A
DRAM Correctable : N/A
DRAM Uncorrectable : N/A
Aggregate
SRAM Correctable : N/A
SRAM Uncorrectable Parity : N/A
SRAM Uncorrectable SEC-DED : N/A
DRAM Correctable : N/A
DRAM Uncorrectable : N/A
SRAM Threshold Exceeded : N/A
Aggregate Uncorrectable SRAM Sources
SRAM L2 : N/A
SRAM SM : N/A
SRAM Microcontroller : N/A
SRAM PCIE : N/A
SRAM Other : N/A
Channel Repair Pending : No
TPC Repair Pending : No
Retired Pages
Single Bit ECC : N/A
Double Bit ECC : N/A
Pending Page Blacklist : N/A
Remapped Rows : N/A
Temperature
GPU Current Temp : 48 C
GPU T.Limit Temp : 40 C
GPU Shutdown T.Limit Temp : -5 C
GPU Slowdown T.Limit Temp : -2 C
GPU Max Operating T.Limit Temp : 0 C
GPU Target Temperature : N/A
Memory Current Temp : N/A
Memory Max Operating T.Limit Temp : N/A
GPU Power Readings
Average Power Draw : 28.81 W
Instantaneous Power Draw : 35.39 W
Current Power Limit : 360.00 W
Requested Power Limit : 360.00 W
Default Power Limit : 360.00 W
Min Power Limit : 250.00 W
Max Power Limit : 360.00 W
GPU Memory Power Readings
Average Power Draw : N/A
Instantaneous Power Draw : N/A
Module Power Readings
Average Power Draw : N/A
Instantaneous Power Draw : N/A
Current Power Limit : N/A
Requested Power Limit : N/A
Default Power Limit : N/A
Min Power Limit : N/A
Max Power Limit : N/A
Power Smoothing : N/A
Workload Power Profiles
Requested Profiles : N/A
Enforced Profiles : N/A
Clocks
Graphics : 255 MHz
SM : 255 MHz
Memory : 810 MHz
Video : 645 MHz
Applications Clocks
Graphics : N/A
Memory : N/A
Default Applications Clocks
Graphics : N/A
Memory : N/A
Deferred Clocks
Memory : N/A
Max Clocks
Graphics : 3090 MHz
SM : 3090 MHz
Memory : 15001 MHz
Video : 3090 MHz
Max Customer Boost Clocks
Graphics : N/A
Clock Policy
Auto Boost : N/A
Auto Boost Default : N/A
Fabric
State : N/A
Status : N/A
CliqueId : N/A
ClusterUUID : N/A
Health
Summary : N/A
Bandwidth : N/A
Route Recovery in progress : N/A
Route Unhealthy : N/A
Access Timeout Recovery : N/A
Incorrect Configuration : N/A
Processes
GPU instance ID : N/A
Compute instance ID : N/A
Process ID : 3982
Type : C
Name : …/kit
Used GPU Memory : 18 MiB
Capabilities
EGM : disabled

’
2025-09-17T10:36:45Z [134ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] osDistro = ‘ubuntu’
2025-09-17T10:36:45Z [135ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] osName = ‘22.04.5 LTS (Jammy Jellyfish)’
2025-09-17T10:36:45Z [136ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] osVersion = ‘22.04.5’
2025-09-17T10:36:45Z [137ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] portableMode = ‘0’
2025-09-17T10:36:45Z [138ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] primaryDisplayRes = ‘3440x1440x32bit@60Hz’
2025-09-17T10:36:45Z [139ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] runEnvironment = ‘Individual’
2025-09-17T10:36:45Z [141ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] runningInContainer = ‘1’
2025-09-17T10:36:45Z [142ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] shaderdb_debugSymbols = ‘0’
2025-09-17T10:36:45Z [143ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] shaderdb_dumpIncludeOverrides = ‘0’
2025-09-17T10:36:45Z [144ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] shaderdb_dumpIntermediates = ‘0’
2025-09-17T10:36:45Z [145ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] shaderdb_obfuscateCode = ‘1’
2025-09-17T10:36:45Z [146ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] shaderdb_optimizationLevel = ‘1’
2025-09-17T10:36:45Z [147ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] systemInfo = ’
|---------------------------------------------------------------------------------------------|
| Driver Version: 580.65.06 | Graphics API: Vulkan
|=============================================================================================|
| GPU | Name | Active | LDA | GPU Memory | Vendor-ID | LUID |
| | | | | | Device-ID | UUID |
| | | | | | Bus-ID | |
|---------------------------------------------------------------------------------------------|
| 0 | NVIDIA GeForce RTX 5080 | Yes: 0 | | 16303 MB | 10de | 0 |
| | | | | | 2c02 | 48c397f4.. |
| | | | | | 1 | |
|=============================================================================================|
| OS: 22.04.5 LTS (Jammy Jellyfish) ubuntu, Version: 22.04.5, Kernel: 6.14.0-29-generic
| XServer Vendor: The X.Org Foundation, XServer Version: 12101011 (1.21.1.11)
| Processor: Intel(R) Core™ i7-14700KF
| Bare Metal Cores: 20 | Bare Metal Logical Cores: 40

Available Cores: 28
Total Memory (MB): 31870
Total Page/Swap (MB): 8191
---------------------------------------------------------------------------------------------
’
2025-09-17T10:36:45Z [148ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] telemetrySessionId = ‘13986527682965311951’
2025-09-17T10:36:45Z [150ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] terminatedByAbort = ‘0’
2025-09-17T10:36:45Z [151ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] totalRamBareMetalMB = ‘31870’
2025-09-17T10:36:45Z [152ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] totalRamLimitedMB = ‘31870’
2025-09-17T10:36:45Z [153ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] totalSwapBareMetalMB = ‘8191’
2025-09-17T10:36:45Z [155ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] totalSwapLimitedMB = ‘8191’
2025-09-17T10:36:45Z [156ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] userId = ‘default’
2025-09-17T10:36:45Z [157ms] [Warning] [carb.crashreporter-breakpad.plugin] [crash] workingDirectory = ‘/isaac5/isaacsim/_build/linux-x86_64/release’
2025-09-17T10:36:45Z [158ms] [Fatal] [carb.crashreporter-breakpad.plugin] [crash] Thread 3982 backtrace follows:
2025-09-17T10:36:45Z [165ms] [Fatal] [carb.crashreporter-breakpad.plugin] 000: libc.so.6!__sigaction+0x50 (??:?)
2025-09-17T10:36:45Z [170ms] [Fatal] [carb.crashreporter-breakpad.plugin] 001: libgpu.foundation.plugin.so!carbOnPluginStartup+0x4374 (??:?)
2025-09-17T10:36:45Z [174ms] [Fatal] [carb.crashreporter-breakpad.plugin] 002: libomni.kit.renderer.plugin.so!void std::vector<void*, std::allocator<void*> >::_M_realloc_insert<void* const&>(__gnu_cxx::__normal_iterator<void**, std::vector<void*, std::allocator<void*> > >, void* const&)+0x5e34 (??:?)
2025-09-17T10:36:45Z [178ms] [Fatal] [carb.crashreporter-breakpad.plugin] 003: libomni.kit.renderer.plugin.so!carbOnPluginPostShutdown+0x104e (??:?)
2025-09-17T10:36:45Z [181ms] [Fatal] [carb.crashreporter-breakpad.plugin] 004: libomni.kit.renderer.plugin.so!carbOnPluginPreStartup+0x674e (??:?)
2025-09-17T10:36:45Z [186ms] [Fatal] [carb.crashreporter-breakpad.plugin] 005: libcarb.eventdispatcher.plugin.so!carbOnPluginRegisterEx+0x3441 (??:?)
2025-09-17T10:36:45Z [907ms] [Fatal] [carb.crashreporter-breakpad.plugin] 006: libomni.kit.loop-isaac.plugin.so!omni::kit::RunLoopThread::update()+0x114d (/isaac5/isaacsim/_compiler/gmake2/omni.kit.loop-isaac.plugin/../../../source/extensions/omni.kit.loop-isaac/plugins/omni.kit.loop/RunLoopRunner.cpp:348)
2025-09-17T10:36:45Z [917ms] [Fatal] [carb.crashreporter-breakpad.plugin] 007: libomni.kit.app.plugin.so!+0x235e1
2025-09-17T10:36:45Z [923ms] [Fatal] [carb.crashreporter-breakpad.plugin] 008: libomni.kit.app.plugin.so!carbOnPluginPreStartup+0x1fa0 (??:?)
2025-09-17T10:36:45Z [926ms] [Fatal] [carb.crashreporter-breakpad.plugin] 009: kit!+0x3cd3
2025-09-17T10:36:45Z [932ms] [Fatal] [carb.crashreporter-breakpad.plugin] 010: libc.so.6!__libc_init_first+0x90 (??:?)
2025-09-17T10:36:45Z [938ms] [Fatal] [carb.crashreporter-breakpad.plugin] 011: libc.so.6!__libc_start_main+0x80 (??:?)
2025-09-17T10:36:45Z [940ms] [Fatal] [carb.crashreporter-breakpad.plugin] 012: kit!_start+0x25 (??:?)
Segmentation fault (core dumped)

Hi,
If I understand correctly, the exact same scene is working on your other pc but crashes on this one?

Hi BenjaminV,

Yes that’s the case, and it makes me confused. I am wondering if you ever met similar problems and how can I solve it.

Thank you very much :slight_smile:

I do not remember seeing this before. Maybe you can make sure the Nvidia drivers are the same?
That’s clearly a GPU crash.