- Is ZED X One S GMSL version compatible with Holoscan Sensor Bridge that goes into a Thor devkit ?
- I see the ZED Link Mipi Quad, but is there a ZED Link GMSL Quad ?
- If not is there any plans for a GMSL to Mipi Deserializer ?
Hi @snknitheesh,
- Is the GMSL version of the ZED X One S compatible with the Holoscan Sensor Bridge connected to a Jetson AGX Thor Developer Kit?
No. With the Holoscan Sensor Bridge on the Jetson AGX Thor Developer Kit, the only supported StereoLabs camera is the ZED X One Core. It is a 2.3 MP global shutter MIPI camera, and you can use up to 2 of them through the ZED Link MIPI Quad. Setup guide: ZED Link MIPI Quad on AGX Thor with Holoscan Sensor Bridge.
- I see a ZED Link MIPI Quad; is there a ZED Link GMSL Quad?
Yes, the ZED Link Capture Card Quad exists, but it connects to the Samtec camera connector of the Jetson AGX Orin Developer Kit. The AGX Thor Developer Kit has no CSI/MIPI camera port, so the GMSL2 capture cards cannot be used with it. More details: Can I use GMSL2 cameras with the NVIDIA Jetson AGX Thor Developer Kit?
- If not, are there plans for a GMSL-to-MIPI deserializer?
We cannot share information about future products. To use the ZED X One S with Jetson Thor today, we recommend the ZED Box 2 Max (T4000 or T5000). It has 8 hardware-synchronized GMSL2 inputs and comes with the ZED SDK preinstalled. Third-party Thor carrier boards are also supported with our GMSL2 compatibility drivers.