Hi,
I am using ZED2i camera on my drone for local positioning.
Now I want to use the same camera in an additional task.
I want to use the ZED2i camera for QR code scanning and/or bar code scanning.
Setup:
Jetson Xavier NX Developer Kit / ZED Box 16GB
ZED2i Camera
Pixhawk 6X/6C
1- Is this possible to scan the QR/Bar code using ZED2i camera? 2- If yes, to the above questions, is this possible to scan the QR/Bar code while using the IMU data? 3- How can I do this?
Please do share the example or documentation if this is possible.
Thank you.
Ok. I am looking into these examples. But, is this possible to use the same camera for multiple purposes? For example, getting the IMU data, object detection, collision prevention, and scanning the QR code.