Is there a Live Link Unity Package that works with the ZED SDK 5.0.1?

Trying to work out which version of the Live Link stuff to use - on the releases page - the latest one available says it only goes up to 4.2 -
does that mean we can’t use live link with sdk 5.01 ?
(we’re only on 5.0.1 because we installed via the package manager - add a git repo and that’s what it gave us.)
Thanks

Hi,

There is no breaking changes between the 4.2 and the 5.0 for the live link plugin. You should be able to use it with no issue.

Do not hesitate to write back if that’s the case.

Best,

Stereolabs Support