Is it possible to set up a base and rover antenna for RTK setup on the new Zed Box?

As the headline suggests, I’m trying to find out if there is a way to set up second port here to be able to set this up as an RTK base station. We have the one antenna input which is nice, but we are looking to a second so we can have both a base and rover on this machine. We are currently using a second machine to do this. It would greatly simplify things if it is at all possible.

Hi @someguy
Welcome to the StereoLabs community.

Unfortunately, this is not an available solution.

We can only support RTK as explained in the GNSS documentation:

Appreciate the reply. Is there a chance you guys will add this capability in the future? Do you guys just have that Zed-F9P chip installed under the hood? We have a base station that we are running on another machine right now, and I’m just trying to figure out if I can just hook up the second over USB to consolidate things. Not having to manage 2 machines clock times would be wonderful.

This capability requires a hardware upgrade; we will consider it for future versions of the ZED Box.