Hi,
I’m traying to export a .svo file with the code in svo_export.py but I got the error INVALID SVO FILE. I have the right path to the svo file.
What can I do to solve this?
Thanks !
Hi,
I’m traying to export a .svo file with the code in svo_export.py but I got the error INVALID SVO FILE. I have the right path to the svo file.
What can I do to solve this?
Thanks !
Hi @cdforigua05
can you post the path that you are using?
I suppose there’s a problem with it.
Sure !
I tried two paths:
/media/user_home2/mcescobar/Ego-Exo3D/escalada/competencia1/franja_14/grabacion_1.svo
./escalada/competencia1/franja_14/grabacion_1.svo
Thank you for the help !
Can you test the SVO recording with ZED Explorer to exclude any other problems?
I tyied with ZED explorer but it says that I need a GPU to open the files. Which is weird because can open other .svo files.

Thanks
If the SVO is encoded using H264 or H265 the GPU is required for encoding