Integrating custom object detector (YOLOX) with ZED depth sensing API

Hi,

I’m working on a vision-based warehouse automation project using the ZED X Mini camera and ZED Box Mini (Orin NX). We’re developing a system that needs to detect and analyze objects like pallets and racks using a custom object detector (YOLOX) along with the ZED SDK’s depth sensing.

I have a few questions:

  1. Is it possible to combine a custom 2D object detector (like YOLOX) with the ZED SDK depth data, for example, running detection on RGB frames and then querying the depth map for those bounding box regions?

  2. For objects such as pallets or racks, could the depth API be used to infer details like:

    • surface irregularities (e.g., bumps or asymmetric loads on top of a pallet),

    • stacked pallets, or

    • rack occupancy / empty slots (using depth or volume estimation)?

  3. Is there a recommended workflow or example for fusing custom object detection outputs with ZED depth data to extract spatial or volumetric insights?

Any guidance, references, or example pipelines on integrating a depth map with an external detector would be really helpful.

Thanks!
— M

Hi @ms12
Welcome to the Stereolabs community.

Yes, this is available with the ZED SDK.
Please read these sections of our documentation:

This depends on the required accuracy and precision. Normally, you can use Computer Vision processing to perform this type of analysis.

Please explore our GitHub repository with examples and tutorials:

1 Like