Hi there,
I currently use the ZED SDK 5.0 in Python with both depth sensing and object detection enabled. My object detection uses CUSTOM_YOLOLIKE_BOX_OBJECTS and a custom onnx file, which I export using Ultralytics’ export function as follows:
from ultralytics import YOLO
YOLO("..path/to/my/model.pt").export(
format="onnx",
simplify=True,
dynamic=False,
opset=13,
imgsz=608
)
I would like to improve my ZED performance. Currently, we are using fp16. How can I use int8 precision with my custom onnx model? I see in the ZED documentation that int8 is supported using allow_reduced_precision_inference = True on my sl.ObjectDetectionParameters() object. I am using this but I’m still in FP16.
How can I use int8 precision with a custom yololike box object model? Do I need to export my onnx in a specific way?
Thanks!