Inquiry about simultaneous use of ZED1 and ZED2

I’m currently trying to use ZED2 and ZED1 simultaneously on my Xavier AGX. When I install and run ZED_wrapper, one of the two disconnects. Could you tell me the file name and contents that need to be modified? please.

Hi @MeerKat98
you must specify the serial number of the camera to open to each launch file in a multi-camera configuration

Hi @MeerKat98
you must specify the serial number of the camera to open to each launch file in a multi-camera configuration

[Discourse post]

Walter

Walter Lucetti
Senior Computer Engineer
SDK / Robotics / HW
Stereolabs Support

Thank you very much for your reply. Could you tell me the name of the file to assign the serial number to?

Are you using ROS or ROS 2?

I’m using ros-noetic.

Please check this example:

Thank you so much for your real-time reply. I will try it. My purchase of ZED is perfect for me. Thank you for your support.

thank you Two zeds were successfully run. However, there seems to be a problem with the terminal window as shown below. Additionally, I want ZED2 to look forward and ZED1 to look downward. Is the file that adjusts the parameters for this the zed_multi_cam.launch file?
Additionally, please check the log file I attached.
zed_multi_cam_launch_log.txt (38.9 KB)

“[ WARN] [1728917191.737748681]: Camera model does not match user parameter. Please modify the value of the parameter ‘camera_model’ to ‘zed2’
[ WARN] [1728917191.962353671]: Camera model does not match user parameter. Please modify the value of the parameter ‘camera_model’ to ‘zed’”
this and
"[ WARN] [1728917200.601437873]: Messages of type 1 arrived closer (0.199942000) than the lower bound you provided (0.500000000) (will print only once) "

Hi @MeerKat98
That’s an example. You must modify it to match your configuration.
The log warnings explain the problem: set the values of the camera_model parameters correctly.