How to save raw point cloud and Spatial Mapping output as PLY files with ZED 2i

Hi Stereolabs team,

Following up on my previous post titled “Question about ZED 2i point cloud, positional tracking, and overlaying external gas sensor data”, I would like to ask for some help with the first simple step of my workflow.

Before I overlay external sensor data onto the reconstructed 3D map, I first want to confirm how to obtain and save:

  1. the raw point cloud from the ZED 2i camera, and
  2. the fused spatial mapping output from the Spatial Mapping module.

My questions are:

  1. What is the simplest way to retrieve the raw point cloud data from the ZED SDK?
  2. How can I save the raw point cloud as a PLY file?
  3. How can I enable the Spatial Mapping module and save the fused spatial map as a PLY file?
  4. For my robot mapping use case, should I use FUSED_POINT_CLOUD instead of MESH if I want to overlay sensor data later?
  5. Is there a simple Python or C++ example that shows how to save both the camera trajectory and the fused spatial map?

At this stage, I only want to confirm that I can successfully save the point cloud and spatial mapping data first. After that, I will move on to overlaying external gas sensor data onto the 3D map.

Thank you very much for your help.

Best regards,
Hong Wei

Hi Hong Wei,

welcome back. All the steps you describe are directly supported by the ZED SDK, so let me answer each question in order.

1. What is the simplest way to retrieve the raw point cloud data from the ZED SDK?

The point cloud is a “measure” that you retrieve after each successful grab() call by using retrieveMeasure() with MEASURE::XYZRGBA (or XYZ if you do not need color). This gives you an organized point cloud aligned with the left image, one 3D point per pixel. You can find all the details here:

and a minimal tutorial here:

2. How can I save the raw point cloud as a PLY file?

The sl::Mat object holding the point cloud can be saved directly by calling its write() function; the output format is selected by the file extension (.ply, .pcd, .vtk, .xyz). For example, in Python:

python

point_cloud = sl.Mat()
if zed.grab() == sl.ERROR_CODE.SUCCESS:
    zed.retrieve_measure(point_cloud, sl.MEASURE.XYZRGBA)
    point_cloud.write("point_cloud.ply")

The “Depth Sensing” sample on our GitHub repository demonstrates exactly this; press the s key while it runs to save the current point cloud:

3. How can I enable the Spatial Mapping module and save the fused spatial map as a PLY file?

You need to enable Positional Tracking first, then Spatial Mapping. Once the area is scanned, call extractWholeSpatialMap() and save the result with the save() function of the Mesh or FusedPointCloud object, selecting MESH_FILE_FORMAT::PLY (ASCII) or PLY_BIN (binary). The full workflow is documented here:

4. For my robot mapping use case, should I use FUSED_POINT_CLOUD instead of MESH if I want to overlay sensor data later?

Yes, I recommend SPATIAL_MAP_TYPE::FUSED_POINT_CLOUD for your use case. Since your gas sensor data will be point-based measurements associated with camera poses, a fused point cloud is the most natural representation to augment; you can simply append your own colored points to it, or attach scalar values to nearby map points. A mesh is preferable when you need surfaces (collision, occlusion, rendering), which does not seem to be your goal. Note that both map types are expressed in the same World Frame used by the Positional Tracking module, so the poses you record will align with the map without any extra transformation.

5. Is there a simple Python or C++ example that shows how to save both the camera trajectory and the fused spatial map?

The “Spatial Mapping” sample (available in both C++ and Python) shows how to enable mapping and save the resulting map:

and this tutorial walks through the code step by step:

There is no dedicated “save trajectory” function, but it is straightforward to add: inside the grab loop, call getPosition() with REFERENCE_FRAME::WORLD and append the timestamp, translation, and orientation quaternion of each sl::Pose to a CSV or TUM-format text file. This gives you a trajectory that is perfectly synchronized with the point clouds and the fused map, which is exactly what you need for the sensor overlay step.

Once these two steps work, the overlay part of your project becomes a simple matter of transforming each gas measurement into the World Frame using the pose recorded at its timestamp.

Hi Myzhar,

Thank you for your previous help.

I am now working on solving questions 1 and 2.

I successfully retrieved the raw point cloud using MEASURE.XYZRGBA. However, my current code only captures one frame and then stops in less than one minute.

I want the ZED 2i to continuously scan and build one complete 3D map while the camera or robot is moving, then save the final map as a PLY file when I manually stop the program.

Should I use positional tracking and spatial mapping instead of saving the point cloud from retrieve_measure()?

Could you please advise which ZED SDK functions or sample code I should use for continuous 3D mapping?

Thank you.

Best regards,
Hong Wei

zed point cloud.cpp (2.0 KB)

Hi @Justinmars

I successfully retrieved the raw point cloud using MEASURE.XYZRGBA. However, my current code only captures one frame and then stops in less than one minute.

This is the expected behavior of your script; there is a break statement at the end of the loop, right after the PLY file is saved, so the program exits after the first valid frame. In any case, this is not the approach I recommend for your use case, see below.

Should I use positional tracking and spatial mapping instead of saving the point cloud from retrieve_measure()?

Yes, exactly. retrieve_measure(MEASURE.XYZRGBA) returns a single-frame point cloud expressed in the camera reference frame; if you save many of them while the robot moves, they will not be aligned. The Spatial Mapping module does exactly what you need: it uses Positional Tracking to estimate the camera pose and fuses the depth information of each frame into a single, consistent 3D map, ingesting new images, depth information, and tracking poses in the background while you simply call grab() in a loop. Stereolabs

For your case, set the map type to SPATIAL_MAP_TYPE.FUSED_POINT_CLOUD, which generates a colored point cloud instead of a mesh; this is also the best choice for overlaying your gas sensor data later, as I mentioned in your previous thread. StereolabsStereolabs

The workflow in Python:

import pyzed.sl as sl

zed = sl.Camera()
init = sl.InitParameters()
init.depth_mode = sl.DEPTH_MODE.NEURAL
init.coordinate_units = sl.UNIT.METER
# A world-oriented coordinate system is recommended for mapping
init.coordinate_system = sl.COORDINATE_SYSTEM.RIGHT_HANDED_Y_UP
zed.open(init)

# 1. Enable Positional Tracking (required by Spatial Mapping)
zed.enable_positional_tracking(sl.PositionalTrackingParameters())

# 2. Enable Spatial Mapping in FUSED_POINT_CLOUD mode
mapping_params = sl.SpatialMappingParameters(
    resolution=sl.MAPPING_RESOLUTION.MEDIUM,
    mapping_range=sl.MAPPING_RANGE.MEDIUM)
mapping_params.map_type = sl.SPATIAL_MAP_TYPE.FUSED_POINT_CLOUD
zed.enable_spatial_mapping(mapping_params)

runtime = sl.RuntimeParameters()

try:
    while True:  # scan continuously, stop with Ctrl+C
        if zed.grab(runtime) == sl.ERROR_CODE.SUCCESS:
            pass  # mapping is fed automatically at each grab()
except KeyboardInterrupt:
    pass

# 3. Extract the whole map and save it as PLY when you stop
fused_pc = sl.FusedPointCloud()
zed.extract_whole_spatial_map(fused_pc)
fused_pc.save("fused_map.ply", sl.MESH_FILE_FORMAT.PLY)

zed.disable_spatial_mapping()
zed.disable_positional_tracking()
zed.close()

Could you please advise which ZED SDK functions or sample code I should use for continuous 3D mapping?

You can find all the details here:

A few practical tips: choose the mapping resolution and range according to the size of the area and the available memory; if the module returns SPATIAL_MAPPING_STATE.FPS_TOO_LOW or NOT_ENOUGH_MEMORY, the mapping stops integrating new data, but you can still extract the 3D model.